This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81402: 关于TUE参数的含义

Part Number: DAC81402


上述高亮的4个指标不太理解

1.Zero-code (negative full scale) error这个是指码值为0时的输出偏差吗?为什么要强调AVSS满量程呢?

2.Full-scale error这个指标的Full Scale指的是40V吗(单极性0到40V或双极性±20V),如果40V范围的的误差是±0.06%,那么±10V的误差是±0.015%吗?

3.Gain Error的单位是%FSR,这也是至40V满量程的误差吗 如果是±10V输出 误差是±0.015%吗?

4.Bipolar-zero (midscale) error 这是指标是指双极性输出时的输出为0V时的误差指标吗 ±0.03%FSR是指40V量程时候的误差吗?

如果±10V输出 这个指标是±0.0075%吗?设定为0V时输出的范围时±0.0075% x 20 = ±0.0015V

我的精度需求是±11V误差优于±5mV,请问使用DAC81402可以实现吗

  • 您好,

    1、Zero-code (negative full scale) error这个误差主要来源是输出放大器不能完全轨至轨输出造成的。即您加载0代码输出会因为输出放大器输出摆幅限制不能完全输出至0,这个gap就是这个误差。在AVSS=0时,就是输出运放单电源供电时,此时这个误差会最大。

    2、Full-scale error就是代码输入全1(满刻度)时 输出电压的偏差。如果输出±10V,那么FSR应该是20V,误差是±0.06%*20V。

    不同输出范围的输出误差,您可以查看下图:

    3、这里同上,输出40V或±20V,FSR是40V,误差是±0.06%*40V;如果输出范围是±10V,FSR就是20V,误差是±0.06%*20V。

    不同量程下的增益误差,请查看下面曲线:

    4、是的,指双极性输出时的输出为0V时的误差指标。这里FSR同上,是指 DACRANGE寄存器设置值。

    我的精度需求是±11V误差优于±5mV,请问使用DAC81402可以实现吗

    如果需要±11V的输出,那么量程需要选择±15V;

     此DAC的TUE是±0.05%

    如果按±15V量程计算TUE是30*±0.05%=±15mV,不满足要求,但是offset error和gain error可以校准,这样应该可以满足您的精度要求,

    下面视频有TUE的定义及计算方法,同时也有校准方法:

    https://training.ti.com/ti-precision-labs-dacs-precision-dac-calibration?context=1139747-1140267-1140260-1140263-1140264

    下面blog也说明了最大值参数即是3σ数据,在典型的高斯分布上,这些边缘情况不太可能发生,所有参数同时是最大值的概率更小。所以也希望这个blog对您对参数是最大值的概率性有个了解:

    https://e2e.ti.com/blogs_/b/analogwire/posts/dac-essentials-how-accurate-is-your-dac