This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: 用ads1299采集波形发生器产生的正弦波 波形感觉奇怪

Part Number: ADS1299


我自己做了个板子,这是四通道的ads1299,输入信号是正弦波(频率1hz  offset : 500mv  amplitude: 250mVPP)如图红圈所示,造成这种现象的原因是啥?

  • 您好,波形发生器输出的正弦波在没有被ADS1299采集之前,波形是正常的吗?

    上图中的正弦波是在靠近ADS1299的输入端测试的吗?

    看起来是信号发生了反射造成了信号不平滑,但是奇怪的是又都是在波峰或波谷的位置。

  • 谢谢你,我用的是ADS1299_4,采用的是5V供电,四个通道的负极接到了一起。我测试过DC和内部产生的方波,它是正确的。

  • 我想问下输入正弦波的波形,在未和ADS1299 接之前的波形是否正常的?

    您所给的图形,是否是在靠近ADS1299的输入端测试的?用示波器测试下ADS1299的输入。

    从而确定是波形发生器的输出本来就是这样,还是因为和ADS1299连接之后的波形出现了这样。