This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7731: 焊接的电路板芯片上电时一个固定电压

Part Number: DAC7731


您好,我焊接了30块DAC7731EC,每块用到3片,焊接后,其中26块正常工作,有4块电路板中的DAC7731有一个或者两个上电输出固定电压不能正常工作,更换新的芯片又可以正常工作,怀疑是焊接过程损坏,查阅手册,DAC7731的焊接温度是260度,我们板卡焊接采用的回流焊接温度是245°,请帮忙分析下原因!万分感谢!

  • 您好,应该是焊接过程损坏的。 MSL等级是显示最高回流焊温度能到260度,但这个温度焊接只能持续十几秒或几十秒。有些数据手册给出260度peak 焊接温度10s。

    另外,新的非密封表面贴装器件的湿度和回流温度敏感度分类根据当时的 IPC/JEDEC J-STD-020标准修订版。峰值回流温度为根据封装厚度和封装塑料体积指定。无铅工艺IPC/JEDEC J-STD-020标准中的分类温度(TC)表列出无铅工艺的温度。

    参考这篇应用手册Table2和Table3:https://www.ti.com/lit/an/spraby1a/spraby1a.pdf

    另外,您参考第5部分的介绍:作为初始起点、图3所示的回流焊曲线235°C - 250°C可作为典型范围为客户作为峰值回流温度(TP)。 对于客户生产回流焊工艺、峰值回流焊温度(TP)必须较低分级回流温度(TP)、如表2和图3所示。