This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A02: 能否条件触发转换,比如发命令快速启动转换

Part Number: ADS131A02


    

在调试ADC131A02的时候无法实现如下想法:

    我想在周期为1ms的PWM上升沿开始转换数据,也就是我在软件中PWM高电平的时候,启动转换,这样每个采样点距离PWM上升沿的时间都是固定的。

目前达到的状态:

   目前我只是实现了ADC启动后自动连续转换,无法控制采样的位置,也就是目前16KHZ的采样率, 8个采样点可能出现在PWM 高电平的任何地方,而且两个波形的相对位置来回移动。

请问目前的wakeup 命令唤醒大概是多久呢、测试了下,要20ms以上左右,无法实现1ms内来采样和同步。