This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS1298使用双电源供电,当N端有导联脱落时,寄存器LOFF_STATN读到的值始终为0x00,换为单电源供电读取到的状态正常,配置 相关通道的LOFF_FLIP寄存器让导联脱落翻转时读取的状态也正常,请给予帮助,多谢!
电路原理图
寄存器配置
导联脱落读到的状态字
是的,这两个帖子说的是同一个问题,这三个字节是在连续读模式下返回的216个位中的前24个位,第一个字节的低四位和第二个字节的高四位是LOFF_STATP寄存器的内容,第二个字节的低四位和第三个字节的高四位是LOFF_STATN寄存器的内容。
在使用±2.5V供电时,您可以在RA导联断开时,实际测量一下RA输入处的电压吗?同时也测量一个正极输入(比如ECG_C1)导联脱落处的电压看是多少?
这个阈值电压是以供电电压AVDD-AVSS为百分比的,我不太确定这个负极侧 15%是怎样计算的
这个是测量到的电压,未脱落时电压基本上为电源正负峰值的一半,双电源供电都为0V左右,单电源供电都为1.5V左右。脱落时单电源供电引脚电压降落到零点几伏,双电源供电有正有负,正电压都能检测到,RA端为负电压,还是检测不到脱落。
这个用的是私有封装,我看了下,引脚顺序和标准的对不上,但是焊上之后和实际的是对应的。如果使用双电源,C73、C81这些排容是的负极是该接模拟地呢?还是该接-AVSS呢?
接模拟地,我看您接的应该是模拟地;
在导联脱落时,单电源供电时,现在实际结果不管INXP输入端还是INXN输入端都是接近0V。正确的结果应该是:INXP输入端测得电压应该是接近3V,INXN输入端测得电压应该是接近0V。因为根据测量原理,INXP输入端在导联脱落时应该被拉至AVDD使输出饱和,INXN输入端在导联脱落时应该被拉至GND,使输出负向饱和输出0V。
在导联脱落时,双电源供电时,同样的道理,INXP输入端测得电压应该是接近2.5V,INXN输入端测得电压应该是接近-2.5V。
建议您去掉外接的二极管,或者去掉全部输入管脚外接的组件,使输入管脚真正悬空,看导联脱落检测结果怎样?
另外,外加供电电源后,实际测量一下电压是否为期望值。