使用ADS7828,3.3V供电,内部电压基准。由于兼容设计,8个输入通道中,有4个输入通道可以选择使用或者不使用。当不使用时,输入通道上会有一个5V电压串联10K电阻连接到输入通道,高于DATASHEET推荐的3.5V(3.3V+0.2V)电压。问题:1、当内部基准没有打开时,芯片10脚(REF)上会串入输入通道上的5V电压,测量有4V左右,请问是否会对芯片可靠性产生影响?2、当内部基准打开,ADC正常工作时,不使用通道上的高电压是否会对工作通道的采样精度产生影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用ADS7828,3.3V供电,内部电压基准。由于兼容设计,8个输入通道中,有4个输入通道可以选择使用或者不使用。当不使用时,输入通道上会有一个5V电压串联10K电阻连接到输入通道,高于DATASHEET推荐的3.5V(3.3V+0.2V)电压。问题:1、当内部基准没有打开时,芯片10脚(REF)上会串入输入通道上的5V电压,测量有4V左右,请问是否会对芯片可靠性产生影响?2、当内部基准打开,ADC正常工作时,不使用通道上的高电压是否会对工作通道的采样精度产生影响?
Hi Liang,
就如你提到的,ADS78288的输入端电压不能超过电源电压的0.2V,否则:
1) 影响芯片的物理可靠性;
2)影响芯片的正常转换工作(此时ADC转换会出现异常,REF都异常了)
故建议你按照ADS7828器件手册推荐的应用。对于此例,可以把5V分压到1V进行检测即可。谢谢。
Liang
手册上标定的数据都是经过测试后给出的结论,是能保证长时间工作的。如果超出了手册的制定范围,会影响可靠性的