This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:DAC5672芯片数据转换的问题

Other Parts Discussed in Thread: DAC5672, DAC5672A

使用DAC5672做数据转换,FPGA与DAC5672相连,输出数据和写、时钟信号。

目前写和读写时钟信号都是6.25MHz,并且同相位。

14位数据都为高电平,按理说输出的模拟信号应该是一个1.2V的高电平,但是现在输出端没有任何信号。

mode为Dual-BusData,sleep也设置的对的。

请专家帮忙看看怎么回事,是不是与PCB走线有问题。

下面是相关的电路原理图,图上高地位弄反了,但是如果全为1的话,应该没有影响的吧。