Other Parts Discussed in Thread: TLC2543, MSP430F5438
TLC2543 AD芯片采用5V电压,VIH=2V VIL=0.8V VOH=4.9V VOL=0.1V
MSP430采用3.3V电压,VIH=2.64V VIL=0.6V VOH=2.7V VOL=0.6V
由于MSP430输出高低电平满足TLC2543输入高低点平要求,我在原理图中打算直接连接。
芯片连接问题:
(1)这样直接连接是否可行?
(2)MSP430芯片I/O口上电后初始状态是输入还是输出?
(3)如果可以的话,对3.3V和5V电压上电时序是否有要求?存不存在由于电压上电速率不一样,电源平面倒灌的问题?
AD芯片问题:
(1)AD芯片AIN管脚使用跟随器,这个是必须的么?当原理图前级是仪表放大的时候,是否应该可以省略跟随器了。