This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2543 AD芯片与MSP430连接问题

Other Parts Discussed in Thread: TLC2543, MSP430F5438

TLC2543 AD芯片采用5V电压,VIH=2V     VIL=0.8V      VOH=4.9V     VOL=0.1V

MSP430采用3.3V电压,VIH=2.64V    VIL=0.6V      VOH=2.7V     VOL=0.6V

由于MSP430输出高低电平满足TLC2543输入高低点平要求,我在原理图中打算直接连接。

芯片连接问题:

            (1)这样直接连接是否可行?

            (2)MSP430芯片I/O口上电后初始状态是输入还是输出?

            (3)如果可以的话,对3.3V和5V电压上电时序是否有要求?存不存在由于电压上电速率不一样,电源平面倒灌的问题?

AD芯片问题:

             (1)AD芯片AIN管脚使用跟随器,这个是必须的么?当原理图前级是仪表放大的时候,是否应该可以省略跟随器了。