This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:ADS1248 IDAC 没有电流

电路如下图:

 

电路原理如下图

参考电压:REF02V

PGA16

IDAC500uA

图中RTDPT100)的滤波电容未接,RTD150欧电阻替代,三线接法,

各寄存器设置如下:

00  1H

01  0H

02  20H

03  42H

04  0H

05  0H

06  0H

07  40H

08  15H

09  40H

0A  84H

0B  1H

0C  0H

0D  0H

0E  0H

 

测试:RTD1-1AIN0导通 RTD1-2RTD1-3AIN1BIAS导通,R1接地端与地导通,模拟地与数字地相通,DVDD4.63VAVDD3.16VRTD1,RTD2,RTD3均无电流,R1两端电压为0

 

问题1

为什么 RTD所有引脚均无电流,R1两端电压为0?

 

问题2

如果正常工作时,使用pt100测温范围是0400度(100-247.98欧),是否满足对模拟端口的电压要求

 

问题3

模拟端口采用电容滤波的电容值是否合适,有什么建议?

 

问题4

如果模拟端口采用RC滤波,是否应接两个端口改为提供IDAC,最多只可以接2PT100