Other Parts Discussed in Thread: ADC3664,
我在文档里看到 “In normal operating mode, the entire ADC full scale range gets converted to a digital output with 14-bitresolution. The output is available in as little as 1 clock cycle on the digital outputs.”,而full scale是3.2VPP,请问是当EVM板子的J2 CHA Input(Balun)为1.6V直流的时候ADC的数字输出为二进制(11111111111111),当该引脚为-1.6V直流的时候数字输出为(00000000000000),当该引脚为0V直流的时候数字输出为(0010000000000000)这样吗?