TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM: ADC3664EVM

Part Number: ADC3664EVM
Other Parts Discussed in Thread: ADC3664,

我在文档里看到 “In normal operating mode, the entire ADC full scale range gets converted to a digital output with 14-bitresolution. The output is available in as little as 1 clock cycle on the digital outputs.”,而full scale是3.2VPP,请问是当EVM板子的J2 CHA Input(Balun)为1.6V直流的时候ADC的数字输出为二进制(11111111111111),当该引脚为-1.6V直流的时候数字输出为(00000000000000),当该引脚为0V直流的时候数字输出为(0010000000000000)这样吗?

  • 您好,

    通过Balun耦合输入是AC耦合输入,直流信号无法通过,如果需要采集直流信号可以将电路调整为FDA 使用直流耦合输入,ADC3664EVM User's Guide第19也有相关调整说明。

    输出数据格式默认是二进制补码形式,如果需要可以通过 register 0x8F and 0x92 配置:

  • 我说错了,我给的是一个正弦波,幅值是3.2VPP,我就是不太清楚输出码流和输入幅度之间的关系。意思就是说,当这个正弦波在某一时刻被采样且采样值为1.6V时是输出14个1吗(14bit=11111111111111)?(正弦波信号接在ADC3664EVM板子的J2 CHA Input(Balun)管脚

  • 您是单端输入是吗?默认二进制补码格式?如果是这样的话,那输出就是14个1。

    ADC3664每个输入(xINP/ xINM)的共模电压要求是0.95V,输入摆幅在0.95V上下0.8V摆动,这样每个管脚的摆动范围是0.15V ~1.75V,摆动幅值是1.6Vpp。差分输入的话,输入范围就是±1.6V,摆动幅值范围就是3.2Vpp。二进制补码格式时,最小输入值是-1.6V,对应输出code是0x2000,最大输入值是+1.6V,对应输出code是0x1FFF。

  • 明白了。还有个问题:

    在ADC3664EVM的使用说明书中(即sbau361.pdf),你们只说analog input最大是3.2VPP,实验中用的是2.8VPP(如图一所示),我理解的就是可以最大输入一个正弦波,其最大值为1.4V,最小值为-1.4V,这个正弦波可以通过图二的J2引脚(balun输入可以实现单端转差分)传递给adc3664芯片。但是你又说需要共模电压0.95V。我现在不明白的就是,这个sample clk(J9引脚)和J2 CHA Input引脚可以接受的电压是多大呢?

    按照你的回答,我理解的就是,对于J2 CHA Input这个管脚,外面的信号发生器最大可以生成一个1.6VPP的正弦波,其中直流偏置是0.95V,也就是说这个正弦波的最小值是0.15V,最大值是1.75V。同理,sample clk(J9引脚)也是最大可以接受这样的一个正弦波(1.6VPP的正弦波,其中直流偏置是0.95V,也就是说这个正弦波的最小值是0.15V,最大值是1.75V)   在这一段中,我说的最大是正常情况下的最大值,而不是absolute maximum rating,如图三所示

    图一

    图二

    图三

    我再补充一下:信号发生器生成一个1.6VPP的正弦波,其中直流偏置是0.95V,也就是说这个正弦波的最小值是0.15V,最大值是1.75V。生成的这个波形应该是算直流信号吧?这样就不可以通过J2进行AC Couple了吧?(如下图所示)

    所以,可以的话请告诉我,外面信号发生器,需要给ADC3664EVM的J2和J9引脚多大的信号呢?(指信号的幅值,最大可以多少伏,最小可以多少伏的一个正弦信号或者方波信号),你在下图中仅用dbm表示,我不清楚电压是要多大

  • 您好,新的问题建议您发新帖以便其他用户进行问题检索,谢谢您的理解与配合。