This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5675的时钟问题

Other Parts Discussed in Thread: DAC5675

尊敬的TI工程师:我是南京航空航天大学的学生,目前正在使用TI公司的高速数模转换芯片DAC5675,在设计中我们使用Xilinx公司的XC2V3000FPGA给DA芯片发送数据,时钟也是FPGA发送,在转换速率高于150MHz时发现模拟信号出现毛刺,我们考虑是FPGA输出的150MHz时钟出现严重抖动导致时钟和数据的时序紧张导致,所以想改进设计,FPGA和DA芯片的时钟由高性能的时钟芯片(一个芯片同时出两路同频同相的时钟)提供,但是又碰到数据是FPGA发送,时钟由时钟芯片提供,时钟和数据的延迟还是没法解决,想请TI的工程师看看这样的设计是否合理,DAC5675的数据和时钟到底怎么设计才算合理?

  • 您好,

    下面是我们工程师的一些反馈:

    1、150MHz的生成速率对于vertex2来说已经不低,所以请他们查看综合后的报告,看是否能满足时序约束要求,也就是XC2V3000是否能保证生成的时钟稳定

    2、150MHz的时钟信号对于PCB布线有一定的要求,比如阻抗匹配方面,时钟线和数据线等长问题,时钟信号和数据信号进行包地处理已减少干扰等

    3、如果使用时钟芯片提供时钟信号,同样会存在上面的2个问题,但是对于时钟和数据的同步我认为不是问题,可以利用时钟的2个沿来分开触发。不清楚DAC5675是时钟的上升沿还是下降沿采样数据,假设是下降沿采样数据,可以让fpga的时钟的上升沿驱动数据输出,这样有半个时钟周期的建立时间和保持时间

    4、不清楚DAC5675是否支持LVDS,如果能,建议使用lvds的信号,这样性能会有较大保证

    5、好像xc2v fpga很老的系列了,如果可能换个4v以上高等级的试试

  • 可以用差分时钟输入到5672中。用逻辑分析仪抓一下时序吧,看看margin够不够了。

  • 麻烦问一下,我现在使用5675A,时钟引脚CLK接到3.3V的CMOS电平上,CLKn通过电容连接到地上,DA输出的时钟为150MHZ,由FPGA提供,FPGA在时钟下降沿打入数据,上升沿开始转换。有时候DA输出有毛刺,和两个时钟引脚的差值400mv-800mv不满足有关系吗?