Hi
Datasheet上谈到LDC1000可以用于Medical Devices,是否可以用于人体测量(use ldc1000 to map the movements or relative position of 2or more targets in human body)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Datasheet上谈到LDC1000可以用于Medical Devices,是否可以用于人体测量(use ldc1000 to map the movements or relative position of 2or more targets in human body)?
楼主:
你好。LDC1000用作medical device现在比较少见,但是LDC1000的应用范围相当广,理论上来说,在有导体接近LDC1000的场合,LDC1000都能使用。比如说齿轮转速的测量,金属的接近距离测量,角度测量,金属按键检测,金属属性分析等。
我感觉LDC1000的测距范围很小的。而且我不清楚怎么进行角度和金属的测量。可以解释一下吗?麻烦的话可以加我QQ983817868
我感觉LDC1000的测距范围很小的。而且我不清楚怎么进行角度和金属的测量。可以解释一下吗?麻烦的话可以加我QQ983817868
您好,LDC应用于轴向距离检测时,有效检测距离约为线圈的直径,为了保证良好的灵敏度最好检测范围是线圈的半径, 如果想提高检测距离,可以使用三角形的金属片在线圈上左右移动的方案,datasheet上面有图片示例。
恩恩 好的,谢谢解答!不过,程序如果能读取各个寄存器的值,就能进行后面的电阻,电感,位移那系列数据的计算了吧?可是我测出LDC1000_CMD_RPMAX(0X01)和LDC1000_CMD_RPMIN(0X02)的十六进制值分别为0X81和0X82,在官方文档LDC1000.PDF里面有个表格“Table 6. Register settings for Rp_MAX”找不到对应的电阻值,那我就没办法根据公式Rp=(RpMAX * RpMIN)/(RpMIN * (1-Y)+RpMAX * Y )来计算Rp了啊?难道是我数据采集错了?
电阻是根据寄存器输出的ProximityData(address:0X22,0X21)的值计算的,电感是根据Fcount(address:0X23 through 0X25)的值计算的,具体计算公式参考datasheet;RPmax和RPmin是在测量谐振电阻之前写入寄存器设置RP测量范围的,测量方法可参照datasheet,不同的测量范围与分辨率有关,但是不能超出798Ω~3.93MΩ的范围,如果寄存器读取的数据不在这个范围内,请检查谐振LC的设计是否合理,设计不合理会导致LDC内部的震荡电路没法起振。