Other Parts Discussed in Thread: ADS1278
我用ADS1278,8通道,SPI模式,如果用CLK-11.0592Mhz的晶振,SCLK用5MHZ,数据采集正确,若果把晶振(CLK)提高到20M以上,SCK频率提高,采集数据不对,偶尔出现后三通道的数据等于前三通道,请问这是什么原因,CLK与SCLK有严格要求吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
datasheet上面说
“SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK."
请问你的应用中是否满足了这一要求?
请帮解决一下两点疑问:
问题一:SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK."这句话是否可以理解为SCLK必须是连续给出的(如果读8通道就是连续的192个SCLK),而且必须严格遵守1, 1/2, 1/4, and 1/8的比例限制?那为什么我用11.05992MHZ的 fCLK,5MHZ和9MHZ的SCK均能读到正确的数据。
问题二:如果用CPU自带的SPI接口,分24次采集,每次采集8bit,这样是不是就不满足“SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK”这个要求了?(我用两种方式IO模拟的时序和CPU自带SPI)
一,SCLK must be continuously running 。。。这个应该是SCLK在ADC运行阶段一直都有,不受~CS控制。换句话说,不是~CS为低时SCLK才被送出去。
二,11.05992MHz的问题,应该是SPI在设计时候留了一定的裕度,所以可以适应的fclk范围比datasheet上写的更宽。但是保险起见,还是遵照datasheet上的说明为好。
三,可以试试,但是估计不行。