This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278 的CLK与SCLK的关系

Other Parts Discussed in Thread: ADS1278

我用ADS1278,8通道,SPI模式,如果用CLK-11.0592Mhz的晶振,SCLK用5MHZ,数据采集正确,若果把晶振(CLK)提高到20M以上,SCK频率提高,采集数据不对,偶尔出现后三通道的数据等于前三通道,请问这是什么原因,CLK与SCLK有严格要求吗?

  • datasheet上面说

    “SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK."

    请问你的应用中是否满足了这一要求?

  • 不知道你处将SCLK提高到多少,要求SCLK 不可以大于CLK频率;请对照数据手册P8中的要求检查时序与时间要求

  • 请帮解决一下两点疑问:

    问题一:SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK."这句话是否可以理解为SCLK必须是连续给出的(如果读8通道就是连续的192个SCLK),而且必须严格遵守1, 1/2, 1/4, and 1/8的比例限制?那为什么我用11.05992MHZ的 fCLK,5MHZ和9MHZ的SCK均能读到正确的数据。

    问题二:如果用CPU自带的SPI接口,分24次采集,每次采集8bit,这样是不是就不满足“SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK”这个要求了?(我用两种方式IO模拟的时序和CPU自带SPI)

  • 一,SCLK must be continuously running 。。。这个应该是SCLK在ADC运行阶段一直都有,不受~CS控制。换句话说,不是~CS为低时SCLK才被送出去。

    二,11.05992MHz的问题,应该是SPI在设计时候留了一定的裕度,所以可以适应的fclk范围比datasheet上写的更宽。但是保险起见,还是遵照datasheet上的说明为好。

    三,可以试试,但是估计不行。

  • 您好! 手册上提到For best performance, limit fSCLK/fCLK to ratios of 1, 1/2, 1/4, 1/8, etc. SCLK的频率不是严格受到比例的限制,请问您的SCLK频率提到多少? 另采集到的前三个通道的数据是正确的吗? 一共采集了8个通道?

  • 我用的是27M晶振,SCLK的频率是5Mhz,采集到前三通道数据正确,后边数据不对。晶振频率变小,采样通道数正确率变高。

  • 如果采用27M的CLK,TDM单通道SPI输出,高速模式的输出的data rate为105KSPS, 8个通道,24bit输出的话,SPI的时钟要求要大于105K*8*24=20MHz,所以5HMz的SPI时钟不能满足要求