TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM: ADC3664EVM

Part Number: ADC3664EVM
Other Parts Discussed in Thread: ADC3664, , CDCE6214

你好,在ADC3664EVM中,采样时钟可以通过J9 balun input进行输入,也可以通过FPGA产生信号时钟,请问如果使用FPGA产生采样时钟给ADC3664的话,下图中的原理图需要进行怎样的修改呢?包括哪些DNP需要重新焊接连接之类的。如果我不需要接受FPGA_REFCLK的话,是不是就只用焊接R39呢?也就是FPGA_CLK。对这个FPGA_CLK有什么幅度需求吗?也就是FPGA这边关于FPGA_CLK这个输出信号引脚有什么配置需求吗,包括电气特性之类的

还有一个问题,在ADC3664EVM手册(sbau361.pdf)中讲解到,使用板载时钟就会进行频率锁定。请问这个板载时钟是不是EVM板子上的10M时钟?如果我将ADC配置成14bit 1-wire  real decimation,decimation factor=8的话,那么这个板载时钟频率够吗?不清楚怎么配置板载时钟

  • 您好,

    请问如果使用FPGA产生采样时钟给ADC3664的话,下图中的原理图需要进行怎样的修改呢?包括哪些DNP需要重新焊接连接之类的。

    请按照下面PPT修改:

    ADC3664EVM_FMC_Clocking.pptx

    电气特性要求:

    板载时钟选项(CDCE6214)无法生成所需频率的DCLKIN,这将在下一次PCB修订中删除。

  • 你好,按照PPT进行修订后,由FPGA提供的FPGA_CLK是单端信号而非差分信号,请问这个信号需要什么电气标准?是LCVMOS25吗(即vivado给这个FPGA_CLK需要进行什么样的电气标准配置)。

    按照我个人的理解:由FPGA以LCVMOS25电气标准驱动FPGA_CLK信号,那么根据改版后的电路原理图来看,CLKM恒定为0V,而CLKP将会接收到一个2.5VPP的方波,这个方波的最大值是1.25V最小值是-1.25V,那么根据差分信号Vdiff=Vp-Vn可知,Vdiff的大小也会是一个2.5VPP的方波,最大值为1.25V最小值为-1.25V,这满足最大差分信号3.6VPP。但是我有个疑惑,就是CLKP最小值将到达-1.25V的话,这不是会烧坏芯片吗?如下图所示,最小值只能是-0.3V

    下图为改板后的原理图

    由于目前无法确认FPGA以什么电气标准去驱动FPGA_CLK信号,所以麻烦告知一下,谢谢!

  • 您好,请按照datasheet 中第 8.3.2.1节的要求设计: