ADC3664EVM的采样信号、DCLKIN和模拟输入信号都只是标注了dbm,请问对应的电压幅值是多少VPP?看到文档里说测试时使用的模拟信号是2.8VPP,请问是±1.4V的信号吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM的采样信号、DCLKIN和模拟输入信号都只是标注了dbm,请问对应的电压幅值是多少VPP?看到文档里说测试时使用的模拟信号是2.8VPP,请问是±1.4V的信号吗
您好,
采样时钟差分和共模幅值:

DCLKIN差模和共模幅值:

模拟输入差模和共模幅值:

看到文档里说测试时使用的模拟信号是2.8VPP,请问是±1.4V的信号吗
每个管脚输入的共模电压都是0.95V,上下摆动范围是0.8V,这样每个管脚的输入范围是0.15V ~1.75V;差分输入摆动范围就是±1.6Vpp;
如果模拟输入是2.8Vpp,对应的差分输入就是±1.4Vpp,即在0.95V上下0.7V摆动,那么每个管脚上输入范围就是0.25V~1.65V。