This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC900系列如何单极性输出

Other Parts Discussed in Thread: DAC900

你好,我使用DAC900搭建一个Datasheet里推荐的电路,如下图:

能够正常输出-1V到+1V的波形。然后根据Datasheet所说可以轻易地添加直流偏置:

但是根据差动放大器的传递函数,代入DAC900的输出  如下图:

似乎无法做到改变电阻阻值 使输出为0~2V。(虽然根据公式在R4=0时可以轻易把输出改变为0~ -2V,这个在Tina仿真中也实现了)。

我想知道 如何添加直流偏置使输出为0~2V。