Other Parts Discussed in Thread: ADS1298, ADS1299, TMS320C5515, TMS320F28335
TI 工程师你们好,我最近想做个脑电放大器,先是买了ADS1299EVM开发板,因MMB0当时没原理图(现在已找到),且配套的软件是用LABVIEW 开发,我想用C语言开发,就在你们网上看到用TMS320C5515控制的ADS1298实验平台,又因ADS1299和ADS1298配置相似,所以我就又买了一套TMS320C5515evm开发套件,刚好该套件有ADS1299子板的接口,我查了手册接口完全兼容,所以着手用TMS320C5515控制ADS1299,我用了C5515的CSL库,在SPI控制EEPROM的例子上修改。用GPIO控制RESET ,START和CS,写寄存器后又读寄存器,读寄存器的结果完全正确,但按照ADS1299手册最后配置的流程图设计程序,但发出START指令后(start管脚一直拉低),/DRDY用示波器量取的波形与手册正好反相,如果用C5515的INT1管脚接受/DRDY信号,则会导致不停地来中断,很快就死机了,希望能帮助解决一下,相关程序和波形入附件所示。急需,谢谢!!!!!