This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299 DRDY 反相问题

Other Parts Discussed in Thread: ADS1298, ADS1299, TMS320C5515, TMS320F28335

TI 工程师你们好,我最近想做个脑电放大器,先是买了ADS1299EVM开发板,因MMB0当时没原理图(现在已找到),且配套的软件是用LABVIEW 开发,我想用C语言开发,就在你们网上看到用TMS320C5515控制的ADS1298实验平台,又因ADS1299和ADS1298配置相似,所以我就又买了一套TMS320C5515evm开发套件,刚好该套件有ADS1299子板的接口,我查了手册接口完全兼容,所以着手用TMS320C5515控制ADS1299,我用了C5515的CSL库,在SPI控制EEPROM的例子上修改。用GPIO控制RESET ,START和CS,写寄存器后又读寄存器,读寄存器的结果完全正确,但按照ADS1299手册最后配置的流程图设计程序,但发出START指令后(start管脚一直拉低),/DRDY用示波器量取的波形与手册正好反相,如果用C5515的INT1管脚接受/DRDY信号,则会导致不停地来中断,很快就死机了,希望能帮助解决一下,相关程序和波形入附件所示。急需,谢谢!!!!!

ADS1299配置及波形文件.rar
  • TI工程师你们好,怎么没人回我呀,好多天了!!!我汇报一下最新进展,经过近一段调试,发现了一个奇怪的问题,如果用CSL库的SPI_read函数读数据,那么根据ADS1299文档,需要读27个字节(216位),但我通过多次实验,最多只能读4个字节,如果读的数超过5个字节,则/drdy对应的DSP INT1管脚的电平一直被拉高,而不是经过一个周期出现低电平,不知道怎么回事?我感觉是中断保护,不知道该如何解决???

  • TI 工程师你们好!我的问题怎么没人回复呀???我的最新进展是我用CSL的SPI_read函数读数时,最多只能读4个字节,如果超过5个字节,则/DRDY管脚被一直拉高,我怀疑是中断保护,怎样才能正确读27个字节(216位),请工程师们帮忙解决一下,谢谢!!!

  • 你好,问一下,你的这个配置ADS1299的操作是在ADS1299EVM开发板上完成的吗,我在写寄存器后又读寄存器时总是读到E000,想问一下,你读ID读出的结果是什么,ADS1299EVM开发板的MMB0和FE是连接在一起进行的还是单独调FE板的。

    最后还想问一下,能不能把MMB0的原理图发我一份,我的邮箱是755512696@qq.com,谢谢啦

  •  你好,

    楼主,我用的tms320f28335,控制ada1299现在我能检测到内部的测试方波,但是外接信号发生器时,却检测不到信号,楼主现在做的怎么样了, 能不能加个q,交流一下啊,万分着急。

  • 您好

      我也是在用ADS1299的,不知道您现在的进度怎么样,MMB0的原理图可以给我发一份吗?

      希望可以加您的QQ 探讨一下

       QQ。1187245816

  • 你好!我最近也在用1298r的前端板和MMB0板做调试。你说的START脚据我所知是用于多个芯片使用时的同步控制用的,不知你这里是否用对了?另外,DRDY的低电平指示ADC转换数据有效,这个信号会持续一段时间,你C5515中的终端应该用边缘触发模式,不能用电平触发模式,否则就会不停地中断。

    希望与你继续交流!

    我需要MMB0的原理图,请你发到我的邮箱:krzx45815@sina.cn, 万分感谢!

  • 您好,请问您找到母板的原理图了吗,方便发我一份不?1138579250@qq.com