REF200规格书里有如下应用电路:
我欲将其用到PT1000温度测量中,PTA和PTB即PT1000的两端点,如下电路图:
问题是PT_ADC处电压总不正确,譬如25mV/1.034V/1.251V随机发生。按照理论算法,PT_ADC处电压为: 100uA * 1000R * 21 = 2100mV.
又用万用表量的PTA和PTB两端电压为0,理论值应该是 100uA * 1000R = 100mV.
所以请教专家我的电路问题出在哪?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你这里的问题是供电,这三个芯片应改成正负双电源供电,因为你的电流方向会在RT1000上形成一个负电压,单电源供电是不行的。
Roffset一般取值为PT1000所测温度的中间值,实际也可以不加Roffset,可以根据你的需要和测温范围进行选择。关于Roffset,下面的paper测温有相关的介绍。
请问有没有负电压输出的LDO电源管理IC呀?就好像HT7130-1的那种IC,只是它是正输出,我要的是负输出的,如果哪位大哥知道,请告知型号?小弟十分感谢!并把仅有20分全部奉上。(不要像79L05那种,其静态工作电流好大。)
输出电流只要能达到30mA即可,之所以指定要LDO,就是想让它的静态电流达到最小。另外,我说的负输出是指负输入,输出也是负,也就是把正作为公共线。价格越便宜越好,谢谢!
你可以把REF200电流源的方向改变一下,这样也可以实现。