请教“the digital filter rejects both 50Hz and 60Hz signals,completely settles in one cycle”,是指该转换器无法对50Hz或60Hz信号进行转换,会对其进行滤除的意思吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tai,
ADS1245这种ADC就是用来采直流信号的:在2.5MHz时钟速率下典型的转换速率是15SPS, 最大支持6MHz的时钟速率,此时最大的转换速率也不过是36SPS。
由于实际应用场合存在着大量的50Hz、60Hz工频干扰,因此该ADC的滤波器设计中特别对这种干扰进行了抑制。从数据手册 图19可见,在50Hz,60Hz的地方有比较大的衰减(-70dB),这就是是所谓的“the digital filter rejects both 50Hz and 60Hz signals”。
从这个频率响应图中也可以看到:随着频率的升高,衰减越来越大;即使在低频段,增益也是不平坦的。这也说明了这种ADC就是用来采直流信号的。
Br
Martin