使用ADS1220的TI官方开发板测量380欧姆0.01%高精密电阻,软件是我自己写的,设置如下:
16倍增益,外部参考1.62V,DA输出250uA,ain0接dac1,ain1接dac2,50Hz抑制
使用20SPS采集速度,连续测量5个小时,实验室环境,最大跳码(也就值最大码值减去最小码值)会有3235个码,换算成温度就是0.53℃,请问这可能是哪里的问题?
我实际要设计的是测量PT100的高精度采集卡,分辨率至少要到0.1℃,请问我怎样才能达到这个分辨率呢?谢谢!
望有专家能帮忙解答一下,谢谢!