Other Parts Discussed in Thread: ADS1118
前面发表了一个问题,不甚详细,以这个附件所述为准,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、“而ADCINP和ADCINN的绝度输入电压(在前面所述背景下),最小可比AVSS小0.1v,醉倒可以比AVDD大0.1v;这里的ADCINP和ADCINN的绝度输入电压是相对于avss的吗?”
是的
2、应该这样理解
( AIN0~AIN15 and AINCOM ) with respect to DGND
AINCOM 是公共参考点,看这个图比较清楚
感谢秋之初和John Fu 。
在John Fu 的回答中,有入下疑问:
问题3与4: 不允许浮地输入,需要在输入端加上共模电压,浮地输入会引入大量噪声,同时有可能会对器件噪声损坏
----------------------------------
a “需要在输入端加上共模电压”如何理解?是通过电容或电阻方面接入参考地吗?图1所示可以吗?
b在前面所述供电背景下,接入浮地热电偶信号(浮地)采用图1所示原理图,可否?
问题5:AINCOM with respect to DGND 指的是输入共模电压到0V,因为此时供电为AVDD=+2.5V,AVSS=-2.5V
--------------------------
模拟输入怎么以数字地为参考?
是不是因为avss不为0,系统中只有DGND为唯一的参考0电平,才有AINCOM with respect to DGND的说法