This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7263功耗问题咨询

Other Parts Discussed in Thread: ADS7263
大家好,我最近使用ADS7263,手册上写的功耗如下图所示,是12.0mA+1.1mA=13.1mA,而我实际测试的功耗在55mA,不知道是否正确,感觉有些大了。
我测试功耗的方法如下:
我的电路原理基本是,用FPGA驱动ADS7263,来采集模拟信号,ADS7263采集后将数据传给FPGA,我在电路正常状态下,在总的电源上加个了小电阻,测试电流得出一个值A,然后我将ADS7263拿掉,同样在总的电源上加个了小电阻,测试电流得出一个值B,A-B=55mA.
  • 你好,

    FPGA在不同的工作情况下,消耗是功耗是否也是不同的呢?

    建议直接在ADS7263的供电线路上串联个采样电阻进行测试。

    你的测试过程中 ADS7263 是正常工作的吧?

  • 1.我又做了实验测功耗,我的电路原理基本是,FPGA无程序在系统总的电源上加个了小电阻,测试电流得出一个值A,然后我将ADS7263拿掉,同样在总的电源上加个了小电阻,测试电流得出一个值B,A-B=13mA.这个是静态工作电流,跟手册上差不多。但是之前这样测试ADS7263功耗是55mA,是FPGA中的驱动ADS7263时序有问题吧?这时候FPGA非常热,我觉得ADS7263功耗是55mA的时候,我们的驱动时序有问题吧?;

    2. 没有给ADS7263留出位置串电阻啊,不能再供电线路上串联个采样电阻进行测试

    3. 由于我们也是初步调试ADS7263,驱动时序是按照手册编写的,是不是正常工作不太清楚。

  • 你好,

    还是将FPGA跟ADC之间的接口先调通再测试功耗吧,这样才有参考意义。

    鉴于你说的FPGA发热严重,建议先检测一下硬件连接是否有短路的情况,或者是ADC跟FPGA的电平是否匹配。