This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我现在将MSP430设定为主机,并为4线模式,ADS1259为从机(只有这一个从机),现将MSP430 STE端口与ADS1259 CS端口连接,以控制CS端口,这样理解您的意思正确吗?
另外,参考书上说,在使用4线同步通信时,STE信号被从从机用作发送和接受允许信号,它由主机提供,即STE=0时,该从机被允许接受和发送;手册上说,ADS1259的CS信号在选定该器件时序置低,且在通信过程中需保持低电位。是不是说,如果按照上面接法,在通信时,MSP430的STE信号需一直置低,以满足CS片选作用时所需要的条件和通信过程中CS所需低电位条件?
首先谢谢您的回复。
还有ADS1259 DOUT端口必须接一个下拉电阻才能与MSP430相连接吗?SYNCOUT端口呢,这个端口我没接电阻,直接接地了,这样符合要求吗?