This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274配置为SPI模式,没有SCLK时,DOUT自己还有输出波形

Other Parts Discussed in Thread: ADS1274

问题请教:
使用ADS1274,AVDD为5V,IOVDD为3.3V,REF为2.5V,COREVDD为1.8V,
CLKDIV为高电平,CLK为18MHz,FORMAT配置为001,MODE配置为01,TEST为00,
测试发现,DRDY,有波形输出,
不向ADS1274发送SCLK信号,DOUT自己一直有波形输出,给了SCLK也一样,DOUT波形应该是与SCLK没有关系,不知道是什么问题,
芯片不热,
还请指教,谢谢。