This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5400: There is a problem with the use process

Part Number: ADS5400


hello!

1) the output voltage at the "VCM" pin does not correspond to the passport level of +2.5 V (at the supply voltage of the chip along the "AVDD5" line +5.0 V) and is +3.14B
2) the digital output data of the ADC is strongly distorted
3) - the identification data of the chips (Die revision), read via the SPI bus (0x01), do not correspond to the passport (0x61);
4) - the readings of the integrated temperature sensors of the chips, read over the SPI bus, do not correspond to reality (at +115 ° C), at a real temperature on the chip housing not exceeding +50 ° C\\

How can these problems be solved?

  • 您好,

    这里是中文论坛,您可以使用中文发帖;

    1、您是DC耦合输入吗?各供电电压测试是否正常?您可以附上前端模拟输入电路吗?输入模拟信号幅值是什么?

    2、输出数字信号走线是不是比较长?您可以附上失真波形吗?

    3、

    3) - the identification data of the chips (Die revision), read via the SPI bus (0x01), do not correspond to the passport (0x61);

    这里是什么意思?很抱歉没有看懂,其他寄存器可以正常读写吗?写入后可以正确读出吗?

    4、寄存器0x05您配置的是什么?您读到的0x08寄存器值是多少?

  • hello!

    芯片上面的PG1.2是什么意思     其他年份打字格式没有这个PG1.2  

  • 很抱歉,TI 论坛旨在解决客户在使用TI产品过程中遇到的技术问题,关于芯片上面的PG1.2,建议您请按照以下方式联系客户支持部门,会有客服为您提供帮助。

    • 打开链接https://ticsc.service-now.com/csm
    • 点击申请新的支持下面的提交申请按钮
    • 在新打开的窗口中点击其他下面的创建案例按钮
    • 在打开的表格中您可以使用中文描述您的问题并且递交。