This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: 杂散

Part Number: DAC38J84


1. DAC38J84测试时有杂散和谐波,杂散的大小影响了SFDR,目前输出60/50/70MHz IF点频信号。在这些频点中杂散点均有出现,通过大量测试,这些杂散点有一定规律,下图是60M输出时,频偏-20MHz处的点,频率是40MHz,如将将频宽打到200MHz时会看到其它谐波和杂散点,下图输出60M时有影响的点是40M,对SFDR的影响超过10dB。其它杂散和谐波距离信号远,幅值小,影响不大,目前主要需要解决20M频偏处的杂散点。

详细的问题见下文档中描述,链接:pan.baidu.com/.../18jhcJiCRwHyUzz7wA8V54Q
提取码:1234

2. 如何直接在论坛中上传文档?