This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S06: 单端模式下PGA轨道监测问题

Part Number: ADS124S06


你好:

      我将ADS124S06配置为单端模式,开启了PGA轨道检测,其余为默认配置,但是在状态寄存器中会报 FL_N_RAILN 和 FL_P_RAILN 错误,请问这是正常情况吗?或者说有哪些原因会报这个错误?感谢答复!

  • 不好意思,和上边的原始问题没有关系,是新问题。

  • 您好,内部PGA输出集成了一个输出电压监视器。 如果PGA的输出电压超过AVDD-1.5V或者低于AVSS+0.15V。就证明PGA的输出电压超出了它的正常输出范围。

    比如3V单电源供电,即AVDD=3V,AVSS=GND,也就是说PGA的输出电压范围要保证在0.15V~1.5V范围内,如果低于0.15V或者高于1.5V就会报错。

    监测的几种情况包括:因此您提到的FL_N_RAILN 和 FL_P_RAILN 错误,对应下面几种情况就是PGA输出OUTN低于AVSS+0.15V,OUTP输出低于AVSS+0.15V。

    The PGA output voltage rail monitors are:

    • FL_P_RAILP (bit 5 of the STATUS byte): VOUTP has exceeded AVDD – 0.15 V

    • FL_P_RAILN (bit 4 of the STATUS byte): VOUTP dropped below AVSS + 0.15 V

    • FL_N_RAILP (bit 3 of the STATUS byte): VOUTN has exceeded AVDD – 0.15 V

    • FL_N_RAILN (bit 2 of the STATUS byte): VOUTN dropped below AVSS + 0.15 V

  • 您好,感谢答复,但是我实际测试出的单端电压值在AVSS+0.15V之上,但还是报了这个错误。

  • 用示波器测量下PGA的OUTP和OUTN的波形,看是否在某一时刻有超过AVDD-0.15V或者低于AVDD+0.15V电压的。