Part Number: ADS124S06
你好:
我将ADS124S06配置为单端模式,开启了PGA轨道检测,其余为默认配置,但是在状态寄存器中会报 FL_N_RAILN 和 FL_P_RAILN 错误,请问这是正常情况吗?或者说有哪些原因会报这个错误?感谢答复!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,内部PGA输出集成了一个输出电压监视器。 如果PGA的输出电压超过AVDD-1.5V或者低于AVSS+0.15V。就证明PGA的输出电压超出了它的正常输出范围。
比如3V单电源供电,即AVDD=3V,AVSS=GND,也就是说PGA的输出电压范围要保证在0.15V~1.5V范围内,如果低于0.15V或者高于1.5V就会报错。
监测的几种情况包括:因此您提到的FL_N_RAILN 和 FL_P_RAILN 错误,对应下面几种情况就是PGA输出OUTN低于AVSS+0.15V,OUTP输出低于AVSS+0.15V。
The PGA output voltage rail monitors are:
• FL_P_RAILP (bit 5 of the STATUS byte): VOUTP has exceeded AVDD – 0.15 V
• FL_P_RAILN (bit 4 of the STATUS byte): VOUTP dropped below AVSS + 0.15 V
• FL_N_RAILP (bit 3 of the STATUS byte): VOUTN has exceeded AVDD – 0.15 V
• FL_N_RAILN (bit 2 of the STATUS byte): VOUTN dropped below AVSS + 0.15 V