This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sampling Rate : 250SPS
config1 : 96h
config2 : C2h
config3 : E0h
Application Mode : Daisy-Chain
When 10 chips are connected in series to read 80 channel data, the register value, data length, and status bit value are all correct..
The baud rate of data transmission at this time is 705600Bit/s .
If you continue to add more chips in series, errors will occur in data reading..
Data length, status bit are incorrect. How many chips can be connected in series in ADS1299? Why do data losses occur so frequently?
我想知道您这里所述的软件开销重组具体应该如何做?
很抱歉我们没有参考code提供给您。
想知道,这个菊花链模式中片与片之间的数据传递与接收是如何做的。会不会存在前一片的一些数据还在传输的过程中未完成,但是被接收到的后一片的数据覆盖掉这种情况呢?
在菊花链模式下所有设备所有通道是同步转换数据的,但是转换code在输出时是按如上截图顺序输出的,因此在输出时在一个转换周期内需要完成所有设备所有通道的转换code输出。因此连接的设备越多需要的SCLK的频率越大,以及时读取转换数据,也就是要符合上述截图公式10,否则的话,就会发生后面的转换code就会被新一轮的转换数据覆盖掉。
总数据的长度和各个芯片的状态位都正常,但是输出数据偶尔会发生整片的丢失。
您的意思是有1个或多个ADC转换结果都是0?
您是采用连续转换模式吗?每个采样周期都会出现这种现象吗?出现的位置和ADC数量一样吗?检查下异常ADC的 START和 CLK信号是否有异常?
我感觉像是异常转换结果的ADC的CLK出问题了,可能CLK信号质量不太好,ADC停止转换了。
总数据的长度正常说明SPI通信没有问题,而start信号是置高的,也没有发生变化,因此问题很可能出自CLK信号,建议您持续关注其中一个ADC管脚处的CLK信号的质量,看在ADC输出数据为0s时,CLK信号质量是否有变化