This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3663: 上电后一定需要硬件复位才能使用吗?!

Part Number: ADC3663


如上图所示,ADC3663数据手册中提到了,上电后必须给reset引脚一个高脉冲,让它恢复默认的参数设置。

因为我们现在的FPGA没有多余引脚了,原理图设计时候,只是把reset简单的用2K电阻上拉到1V8(其实它里面也有个21K上拉电阻),没有额外的控制。

这样的话,ADC3663,可以正常使用吗?!