This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS1298上电初始化成功,能正确读写寄存器,测试信号正确,但是在正常情况下完全采集不到心电信号。测试信号正确按理说ADS1298芯片就没有问题,应该就是外围电路的问题。TI的老师们能帮我看看我的电路有问题吗?我寄存器的配置如下:
ID is 92
CONFIG1 is 86
CONFIG2 is 35
CONFIG3 is c0
LOFF is 3
CH1SET is 0
CH2SET is 0
CH3SET is 0
CH4SET is 10
CH5SET is 10
CH6SET is 10
CH7SET is 10
CH8SET is 10
RLD_SENSP is ff
RLD_SENSN is 0
LOFF_SENSP is 0
LOFF_SENSN is 0
CONFIG4 is 2
WCT1 is 1
WCT2 is 2
PACE is 0
RESP1 is 0
正常情况下采集心电信号,完全采集不到。一点信号输出都没有。实在找不出原因所在,麻烦各位老师帮帮忙,非常感谢
关于原理图:
1、17、18脚不使用的话接AVDD:
2、CLKSEL接的是什么?
3、AGND是否与GND单点连接?
我的RA,LL,LA与官方给的ADS1298 ECG FE原理图上的有点不一样,不知道会不会对采集心电有影响。
您是说使用的通道数不一样吗?如果是这样的话,那没什么问题。
另外,前端滤波器截止频率是不是太低了?您使用评估板上的参数再采集信号怎样?
老师您好,我用信号发生器直接连接INP6端,结果输出是满量程,同时,INP端不连接时也是满量程输出。不知道原因在哪里。
您测试时IN6N接的是WCT是吗?如果是的话,因为WCT是其他电极共同作用结果,所以不太好判断。建议您配置使用内部Test Signal看是否可以正确采集?
1、CLKSEL是数字接口,高低电平标准是DVDD,如下高低电平电压范围,请确认下在接AVDD时,电平是否满足下面截图中要求:
4、得到的方波纵坐标是什么?幅值是否正确?
5、和6、这个问题与下面链接问题一样,下面连接问题我关闭了,将在这个帖子中跟进您的回复。
https://e2echina.ti.com/support/data-converters/f/data-converters-forum/783443/ads1298
满幅输出时,寄存器配置是怎样的?
电路图没看出什么问题
老师您好~
ID is 92
CONFIG1 is 86
CONFIG2 is 35
CONFIG3 is cc
CONFIG4 is 00
LOFF is 02
CH1SET is 00
CH2SET is 00
CH3SET is 00
CH4SET is 00
CH5SET is 00
CH6SET is 00
CH7SET is 00
CH8SET is 00
RLD_SENSP is ff
RLD_SENSN is ff
LOFF_SENSP is 0
LOFF_SENSN is 0
WCT1 is f9
WCT2 is c2
PACE is 0
RESP1 is 0
其中只用到了WCT和RLD,其余的PACE 和RESP功能都没有用到。
谢谢老师,期待您的回复,谢谢~
WCT1 is f9
您具体要测什么心电信号?看您WCT1寄存器的配置,好像要测aVF、aVL、aVR信号,但是看您电路图连接是要测胸导联V1~V6。
如果您要测V1~V6信号,WCT1高4位需配置0.
您是使用ECG模拟仪产生的心电信号吗?建议您使用心电模拟仪产生的信号进行测试。
同时也建议您根据下面FAQ增益计算方法调节下RLD运放的增益: