This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8830: 使用fpga驱动时无法获得预期幅值

Part Number: DAC8830
Other Parts Discussed in Thread: OPA727

我使用fpga设计了DAC8830芯片的驱动,仿真时可以看到输出数据是从16'd0到16‘d65535变化的正弦信号,但是实际接入DAC8830芯片以后获得的是一个幅值300mV,3.0V~3.3V变化的正弦信号,超出Vref。

当我使用16'd0作为输入的时候,输出模拟信号值为3.0V,同样超出Vref数值。参考电压通过ref3025芯片提供。VDD通过线性电源模块提供。

  • 您好,

    您可以附上原理图吗?供电电压是多少?实际测量VREF电压是多少?测量输出时接负载了吗?DAC后级加buffer了吗?

  • 好的,供电电压为5V,Vref实测电压2.5V左右,测量输出时参照datasheet的建议,输出电压后级加了一个OPA727跟随,OPA727同样采用5V供电。

    在我测试的过程中,如果把后级OPA727摘掉,输出的波形就和我的预期值完全一致,我现在怀疑是我的电路设计问题。

    检测过程全程测量8810的输出引脚,因为错误输出状态下OPA727的波形为饱和波形。

    我不太会使用论坛上传原理图 :(

  • 上传原理图的话可以直接将文件拖进回复对话框,截图的话直接粘贴过来就行

    OPA727是电压跟随器形式吗?

  • 是的,OPA727为电压跟随器的形式,该部分设计原理图如下所示:

  • 看您的电路图没问题,如您所说“如果把后级OPA727摘掉,输出的波形就和我的预期值完全一致”,那可能是运放硬件方便的问题,您单独测试OPA727电路可以正常工作吗?

    或者您多测试几块板子,以排除焊接问题