This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8830: 使用fpga驱动时无法获得预期幅值

Part Number: DAC8830
Other Parts Discussed in Thread: REF3025, OPA727

我使用fpga设计了DAC8830芯片的驱动,仿真时可以看到输出数据是从16'd0到16‘d65535变化的正弦信号,但是实际接入DAC8830芯片以后获得的是一个幅值300mV,3.0V~3.3V变化的正弦信号,超出Vref

当我使用16'd0作为输入的时候,输出模拟信号值为3.0V,同样超出Vref数值。参考电压通过ref3025芯片提供。VDD通过线性电源模块提供。