This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.现在电路测试测试结果是:
AVDD 3.3V (49, 50, 57, 60) OK
AVSS (3, 6, 9, 37, 40, 43, 46) OK
LVDD 1.8V (35) OK
LVSS (12, 14, 36)
CLKP (58)
CLKN (59) ADCCLK输入10M晶振输入,1X ADCLK输出正常。6X输出正常。
PD (13) L
VCM 输出1.5V
2.RESET管脚连接到FPGA的IO管脚,这个管脚上电默认是高电平。上电后,通过程序控制RESET拉低后,再拉高。
现在寄存器设置CMD45 在PAT_SYNC模式下,示波器测试任何ADC通道都没有信号输出。
我想咨询下:
1.如果VCM和PLL单元的信号输出正常。能表明IC的1.8V模块所以功能是正常?
2.在PAT_SYNC模式下,示波器测试任何ADC通道都没有信号输出是什么原因?
SPI时序中黄色时钟,蓝色RESET,粉色SDATA
蓝色是reset吗?还是cs?不能在写寄存器的时候拉低reset;
PD是拉低的吗?
建议加去耦电路:
1.现在的电气原理图设计中pin57.58按照并上电阻,这样属于DC输入吗?如果差分时钟输入,芯片的CLKN、CLKP必须串联电容形成AC 耦合输入吗?
是的,属于DC耦合;
CLK管脚内部有共模偏置VCM,如果输入时钟信号共模电压与ADC5282 内部共模电压VCM一致则不需要AC耦合,如果不一致,则需要AC耦合滤除输入时钟信号的偏置电压,通过ADC内部偏置电路重新建立符合ADC要求的偏置电压:
2.现在ADC5258对CLKN、CLKP输入电压如下偏置2.04V±500mv。
这样不匹配ADC内部的VCM=1.5V,因此需要AC耦合输入。
刚看了寄存器配置,寄存器25是0001是吗?不能单端配置BITS_CUSTOM1,需要配合CUSTOM_PAT 位使用,如下datasheet 截图处描述: