This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1158/ads1258调试总结

Other Parts Discussed in Thread: ADS1158, ADS1258

  近期一直在调试ads1158,终于能够得到正常的输出,期间在网上查了很多的资料,发现关于ads1158的资料很少,尤其是基于verilog的程序几乎没有,所查的资料大多语焉不详,因此,本着人人为我,我为人人的精神,现在把ads1158的调试心得写出来,希望能够帮助一些开发者,节省开发时间。

  1、在开发初期,由于是中途接手的项目,对硬件熟悉不够,导致耽误了不少时间,具体的硬件原因就不细说了,因为每一个开发者的硬件不可能是一样的,在这里给的建议是:在ads1158这部分的电路,可以根据数据手册来设计。另外,对于ads1158或者1258来说,模拟量是可以通过muxoutp(pin44)和muxoutn(pin43)引出来后自己添加一些信号处理的电路(如放大,滤波等),再由管脚adcinp(pin42)和adcinn(pin41)输入进芯片进行a/d转换,当然也可以在内部直接连接。如果需要在外部进行信号处理的话,在程序设计的时候需要对config0寄存器bit4位置为1(默认值为0)。数据手册上给出了两种外部信号处理的电路,在数据手册的42和43页。

  2、在程序设计的时候,数据手册上给出了一个流程(在数据手册的40页)。具体为:1)reset spi接口。这是非常重要的一步,这也是我调试花的时间最多地方。如果要使芯片能正常工作,首先要使spi能正常工作。在调试前,有必要仔细研究一下spi的时序(数据手册第7页,图1)。复位的步骤是先将cs置高一段时间再拉低,至于置高的时间我也没搞懂,如果按照数据手册上的4096个fclk的话,发现spi的输出线上的数据是乱的,然后我就不断地增加延长的时间,直至spi出现的数据与预想的差不多。sck的信号通过spi master端(可以是单片机、dsp、cpld/fpga等)给出,这里要注意sck的信号是需要的时候再给,而不是一直给的。比如在发送命令、读取寄存器值,或者读取数据的时候。当然,对另外一个管脚cs的控制也很重要,cs的控制也是在需要的时候再拉低,闲时置高。2)把start管脚置为0,停止转换。一般在初始化的时候基本上都是start=0的。3)软件复位芯片。有的是把reset脚通过硬件复位的,由于我们是软件复位的,不熟悉硬件复位的情况,所以对于硬件复位的话,这步可能不需要。4)配置寄存器。配置的值按照数据手册上的说明结合自己的实际需求给出。5)回读寄存器的值。这个步骤在调试的时候很有用,可以作为判断是否正常工作,如果读出来的值与写进去的值一样,说明spi能够正常工作,尤其是可以根据id寄存器的值来判断,因为这个值是固定的。当然,如果程序调试好了,这部分的程序是可以不要的。6)以上的步骤完成后,可以将start置为1,开始转换。7)开始读数据,读的方式按照数据手册上的三种(直接读,命令读,脉冲读)选一种即可,我选的是直接读,根据drdy的管脚来判断。基本上按照以上的流程来操作是没有问题的,不管是基于什么语言开发。在这里再次强调一下首先要保证spi能够正常通讯。

  3、ads1258基本上和1158操作流程是一样的。网上关于1258的例程比1158的多。TI的这两款芯片用好了是高性能ad转换器,用不好能把人折腾死。数据手册一定要细读。我在调试期间在社区里发了两个帖子都烂尾,不知道是我问的问题太简单,还是工作人员太忙,最后也就不了了之。 

  4、以下是基于verilog编写的源代码。cpld的晶振是50M。分频后得到500K作为sck。

module adc(
				clk,
				rst_n,
				cs,
				sck,
				start,
				pwdn,
				drdy,
				miso,
				mosi,
				rst_ad,
				dataout,
				clkout	
				);
input  clk,rst_n;
input miso; //from ad device
input drdy;
output reg start;
output reg rst_ad;
output reg pwdn;
output reg cs;
output sck;
output reg mosi ;//to ad device

reg[15:0] cnt;
output reg clkout;

always @(posedge clk or negedge rst_n)begin
	if (!rst_n)	begin
		clkout <= 1'd0;
		cnt<=16'd0;
	end	
	else if (cnt == 16'd50)	begin
		clkout <=~clkout;
		cnt <=16'd0;
	end	
	else	begin
		cnt <=cnt+1'd1;
	end		
end

assign sck =clkout && flag_sck;//通过一个标志位与clkout与操作后得到sck

reg flag_sck;
reg [15:0]state_spi;
reg [31:0]time_delay1,time_delay2;
always @(negedge clkout or negedge rst_n) begin 
	if(!rst_n) begin 
		cs <=1'd1;
		flag_sck <=1'd0;
		rst_ad <=1'd0;
		pwdn<=1'd1;
		rst_ad<=1'd1;
		state_spi<=16'd0;
		time_delay1<=32'd0;
		time_delay2<=32'd0;
	end 
	else begin 
		case (state_spi)
		16'd0: begin 
			cs<=1'd1;
			flag_sck<=1'd0;
			//start<=1'd0;
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd1: begin 
			if(time_delay1==32'd3000)begin //3000这个值是最后试出来的,如果按照500K的sck来算,远大于数据手册上的4096fclk。
				cs<=1'd0;
				flag_sck<=1'd1;
				time_delay1<=32'd0;
				state_spi<=state_spi+1'd1;
			end 	
			else begin 
				cs<=1'd1;
				time_delay1<=time_delay1+1'd1;	
			end 	
		end 
		16'd2: begin 
			start<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd3: begin 
			if(time_delay2==32'd3000)begin //复位芯片,这个值也是最后试出来的。
				rst_ad<=1'd1;
				time_delay2<=32'd0;
				state_spi<=state_spi+1'd1;
			end 	
			else begin 
				rst_ad<=1'd0;
				time_delay2<=time_delay2+1'd1;	
			end 	
		end 
		16'd4: begin cs <=1'd1;flag_sck<=1'd0; state_spi<=state_spi+1'd1;end
		16'd5: state_spi<=state_spi+1'd1;
		16'd6: state_spi<=state_spi+1'd1;
		16'd7: state_spi<=state_spi+1'd1;
		16'd8: state_spi<=state_spi+1'd1;
		16'd9: state_spi<=state_spi+1'd1;
		16'd10: state_spi<=state_spi+1'd1;
		16'd11: state_spi<=state_spi+1'd1;
		16'd12: state_spi<=state_spi+1'd1;
		16'd13: state_spi<=state_spi+1'd1;
		16'd14: state_spi<=state_spi+1'd1;
		16'd15: state_spi<=state_spi+1'd1;
		16'd16: state_spi<=state_spi+1'd1;
		16'd17: state_spi<=state_spi+1'd1;
		16'd18: state_spi<=state_spi+1'd1;
		16'd19: state_spi<=state_spi+1'd1;
		16'd20: state_spi<=state_spi+1'd1;
		16'd21: state_spi<=state_spi+1'd1;
		16'd22: state_spi<=state_spi+1'd1;
		16'd23: state_spi<=state_spi+1'd1;
		16'd24: state_spi<=state_spi+1'd1;
		16'd25: state_spi<=state_spi+1'd1;
		16'd26: state_spi<=state_spi+1'd1;
		16'd27: state_spi<=state_spi+1'd1;
		16'd28: state_spi<=state_spi+1'd1;
		16'd29: state_spi<=state_spi+1'd1;
		16'd30: begin state_spi<=state_spi+1'd1; end 
		16'd31: begin 
			cs<=1'd0;
			//flag_sck<=1'd1;
			state_spi<=state_spi+1'd1;
		end 
		//write register command
		16'd32: begin 
			flag_sck<=1'd1;
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd33: begin 
			//flag_sck<=1'd1;
			mosi<=1'd1;
			state_spi<=state_spi+1'd1;
		end 
		16'd34: begin 
			mosi<=1'd1;
			state_spi<=state_spi+1'd1;
		end 
		16'd35: begin 
			mosi<=1'd1;
			state_spi<=state_spi+1'd1;
		end 
		16'd36: begin 
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd37: begin 
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd38: begin 
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		16'd39: begin 
			mosi<=1'd0;
			state_spi<=state_spi+1'd1;
		end 
		//config0
		16'd40: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd41: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end 	
		16'd42: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd43: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd44: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end 	
		16'd45: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd46: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end 	
		16'd47: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end 					
		//config1
		16'd48: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd49: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd50: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd51: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end 	
		16'd52: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end 	
		16'd53: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd54: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd55: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//muxsch
		16'd56: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd57: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd58: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd59: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd60: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd61: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd62: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd63: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
      //muxdif
		16'd64: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd65: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd66: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd67: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd68: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd69: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd70: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd71: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//muxsg0
		16'd72: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd73: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd74: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	//
		16'd75: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd76: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd77: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd78: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd79: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//muxsg1
		16'd80: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd81: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd82: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	//
		16'd83: begin //ch12
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd84: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end
		16'd85: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd86: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end
		16'd87: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end		
		//sysred
		16'd88: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd89: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd90: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd91: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end
		16'd92: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd93: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd94: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd95: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//gpioc
		16'd96: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd97: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd98: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	//
		16'd99: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd100: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd101: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd102: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd103: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//gpiod
		16'd104: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd105: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd106: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	//
		16'd107: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end
		16'd108: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd109: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd110: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd111: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		//id
		16'd112: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd113: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd114: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd115: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd116: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd117: begin 
			mosi <=1'd0;
			state_spi<=state_spi+1'd1;
		end	
		16'd118: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end	
		16'd119: begin 
			mosi <=1'd1;
			state_spi<=state_spi+1'd1;
		end
		16'd120: begin 
			cs<=1'd1;
			flag_sck<=1'd0;
			mosi<=1'd0;
			//start<=1'd1;
			state_spi<=state_spi+1'd1;
		end
		16'd121:state_spi<=state_spi+1'd1;
		16'd122:state_spi<=state_spi+1'd1;
		16'd123:state_spi<=state_spi+1'd1;
		16'd124:state_spi<=state_spi+1'd1;
		16'd125:state_spi<=state_spi+1'd1;
		16'd126:state_spi<=state_spi+1'd1;
		16'd127:state_spi<=state_spi+1'd1;
		16'd128:begin state_spi<=state_spi+1'd1;end
		
		16'd129: begin cs<=1'd0;state_spi<=state_spi+1'd1;end
		16'd130: begin flag_sck<=1'd1;mosi<=1'd0;state_spi<=state_spi+1'd1;end
		16'd131: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end
		16'd132: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd133: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end 
		16'd134: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd135: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd136: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd137: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd138: begin state_spi<=state_spi+1'd1;end
		16'd139:begin state_spi<=state_spi+1'd1;end 
		16'd140:state_spi<=state_spi+1'd1;
		16'd141:state_spi<=state_spi+1'd1;
		16'd142:state_spi<=state_spi+1'd1;
		16'd143:state_spi<=state_spi+1'd1;
		16'd144:state_spi<=state_spi+1'd1;
		16'd145:state_spi<=state_spi+1'd1;
		16'd146:state_spi<=state_spi+1'd1;
		16'd147:state_spi<=state_spi+1'd1;
		16'd148:state_spi<=state_spi+1'd1;
		16'd149:state_spi<=state_spi+1'd1;
		16'd150:state_spi<=state_spi+1'd1;
		16'd151:state_spi<=state_spi+1'd1;
		16'd152:state_spi<=state_spi+1'd1;
		16'd153:state_spi<=state_spi+1'd1;//16
		16'd154: begin state_spi<=state_spi+1'd1;end
		16'd155:state_spi<=state_spi+1'd1;
		16'd156:state_spi<=state_spi+1'd1;
		16'd157:state_spi<=state_spi+1'd1;
		16'd158:state_spi<=state_spi+1'd1;
		16'd159:state_spi<=state_spi+1'd1;
		16'd160:state_spi<=state_spi+1'd1;
		16'd161:state_spi<=state_spi+1'd1;
		16'd162:state_spi<=state_spi+1'd1;
		16'd163:state_spi<=state_spi+1'd1;
		16'd164:state_spi<=state_spi+1'd1;
		16'd165:state_spi<=state_spi+1'd1;
		16'd166:state_spi<=state_spi+1'd1;
		16'd167:state_spi<=state_spi+1'd1;
		16'd168:state_spi<=state_spi+1'd1;
		16'd169:state_spi<=state_spi+1'd1;
		16'd170: begin state_spi<=state_spi+1'd1;end
		16'd171:state_spi<=state_spi+1'd1;
		16'd172:state_spi<=state_spi+1'd1;
		16'd173:state_spi<=state_spi+1'd1;
		16'd174:state_spi<=state_spi+1'd1;
		16'd175:state_spi<=state_spi+1'd1;
		16'd176:state_spi<=state_spi+1'd1;
		16'd177:state_spi<=state_spi+1'd1;//40
		16'd178:state_spi<=state_spi+1'd1;
		16'd179:state_spi<=state_spi+1'd1;
		16'd180:state_spi<=state_spi+1'd1;
		16'd181:state_spi<=state_spi+1'd1;
		16'd182:state_spi<=state_spi+1'd1;
		16'd183:state_spi<=state_spi+1'd1;
		16'd184:state_spi<=state_spi+1'd1;
		16'd185:state_spi<=state_spi+1'd1;
		16'd186: begin state_spi<=state_spi+1'd1;end
		16'd187:state_spi<=state_spi+1'd1;
		16'd188:state_spi<=state_spi+1'd1;
		16'd189:state_spi<=state_spi+1'd1;
		16'd190:state_spi<=state_spi+1'd1;
		16'd191:state_spi<=state_spi+1'd1;
		16'd192:state_spi<=state_spi+1'd1;
		16'd193:state_spi<=state_spi+1'd1;
		16'd194:state_spi<=state_spi+1'd1;
		16'd195:state_spi<=state_spi+1'd1;
		16'd196:state_spi<=state_spi+1'd1;
		16'd197:state_spi<=state_spi+1'd1;
		16'd198:state_spi<=state_spi+1'd1;
		16'd199:state_spi<=state_spi+1'd1;
		16'd200:state_spi<=state_spi+1'd1;
		16'd201:state_spi<=state_spi+1'd1;
		16'd202: begin state_spi<=state_spi+1'd1;end
		16'd203:state_spi<=state_spi+1'd1;//66
		16'd204:state_spi<=state_spi+1'd1;
		16'd205:state_spi<=state_spi+1'd1;
		16'd206:state_spi<=state_spi+1'd1;
		16'd207:state_spi<=state_spi+1'd1;
		16'd208:state_spi<=state_spi+1'd1;
		16'd209:state_spi<=state_spi+1'd1;
		16'd210:state_spi<=state_spi+1'd1;
		16'd211:state_spi<=state_spi+1'd1;
		16'd212:state_spi<=state_spi+1'd1;
		16'd213:state_spi<=state_spi+1'd1;
		16'd214:state_spi<=state_spi+1'd1;
		16'd215:state_spi<=state_spi+1'd1;
		16'd216:state_spi<=state_spi+1'd1;
		16'd217:state_spi<=state_spi+1'd1;//88
		16'd218:state_spi<=state_spi+1'd1;
		16'd219:state_spi<=state_spi+1'd1;
		16'd220:state_spi<=state_spi+1'd1;
		16'd221:state_spi<=state_spi+1'd1;
		16'd222:state_spi<=state_spi+1'd1;
		16'd223:state_spi<=state_spi+1'd1;
		16'd224:state_spi<=state_spi+1'd1;
		16'd225:state_spi<=state_spi+1'd1;
		16'd226:state_spi<=state_spi+1'd1;
		16'd227: begin 
			cs<=1'd1;
			flag_sck<=1'd0;
			start<=1'd1;
			state_spi<=state_spi+1'd1;//state_spi<=16'd228;
		end
		
		16'd228:state_spi<=state_spi+1'd1;
		16'd229:state_spi<=state_spi+1'd1;
		16'd230:state_spi<=state_spi+1'd1;
		16'd231:state_spi<=state_spi+1'd1;
		16'd232:state_spi<=state_spi+1'd1;
		16'd233:state_spi<=state_spi+1'd1;
		16'd234:state_spi<=state_spi+1'd1;
		//16'd235:begin state_spi<=state_spi+1'd1;end
		
		16'd235: begin 
			if(drdy==1'd0)begin 
				//cs<=1'd0;
				state_spi<=state_spi+1'd1;
			end 	
		end
		16'd236:begin cs<=1'd0;state_spi<=state_spi+1'd1;end
		16'd237: begin flag_sck<=1'd1; mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd238: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd239: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd240: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd241: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
		16'd242: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd243: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd244: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 
		16'd245: begin state_spi<=state_spi+1'd1;end
		16'd246:state_spi<=state_spi+1'd1;
		16'd247:state_spi<=state_spi+1'd1;
		16'd248:state_spi<=state_spi+1'd1;
		16'd249:state_spi<=state_spi+1'd1;
		16'd250:state_spi<=state_spi+1'd1;
		16'd251:state_spi<=state_spi+1'd1;
		16'd252:state_spi<=state_spi+1'd1;
		16'd253:state_spi<=state_spi+1'd1;
		16'd254:state_spi<=state_spi+1'd1;
		16'd255:state_spi<=state_spi+1'd1;
		16'd256:state_spi<=state_spi+1'd1;
		16'd257:state_spi<=state_spi+1'd1;
		16'd258:state_spi<=state_spi+1'd1;
		16'd259:state_spi<=state_spi+1'd1;
		16'd260:state_spi<=state_spi+1'd1;
		
		/*16'd261:state_spi<=state_spi+1'd1;
		16'd262:state_spi<=state_spi+1'd1;
		16'd263:state_spi<=state_spi+1'd1;
		16'd264:state_spi<=state_spi+1'd1;
		16'd265:state_spi<=state_spi+1'd1;
		16'd266:state_spi<=state_spi+1'd1;
		16'd267:state_spi<=state_spi+1'd1;
		16'd268:state_spi<=state_spi+1'd1;
		
		/*16'd154:state_spi<=state_spi+1'd1;
		16'd155:state_spi<=state_spi+1'd1;
		16'd156:state_spi<=state_spi+1'd1;
		16'd157:state_spi<=state_spi+1'd1;
		16'd158:state_spi<=state_spi+1'd1;
		16'd159:state_spi<=state_spi+1'd1;
		16'd160:state_spi<=state_spi+1'd1;
		16'd161:state_spi<=state_spi+1'd1;*/
		16'd261: begin 
			cs<=1'd1;
			flag_sck<=1'd0;
			flag_rdat<=1'd0;
			state_spi<=16'd228;
		end
		default:state_spi<=16'd0;	
		endcase
	end 
end

			
endmodule 

 

x 出现错误。请重试或与管理员联系。