Other Parts Discussed in Thread: ADS1158, ADS1258
近期一直在调试ads1158,终于能够得到正常的输出,期间在网上查了很多的资料,发现关于ads1158的资料很少,尤其是基于verilog的程序几乎没有,所查的资料大多语焉不详,因此,本着人人为我,我为人人的精神,现在把ads1158的调试心得写出来,希望能够帮助一些开发者,节省开发时间。
1、在开发初期,由于是中途接手的项目,对硬件熟悉不够,导致耽误了不少时间,具体的硬件原因就不细说了,因为每一个开发者的硬件不可能是一样的,在这里给的建议是:在ads1158这部分的电路,可以根据数据手册来设计。另外,对于ads1158或者1258来说,模拟量是可以通过muxoutp(pin44)和muxoutn(pin43)引出来后自己添加一些信号处理的电路(如放大,滤波等),再由管脚adcinp(pin42)和adcinn(pin41)输入进芯片进行a/d转换,当然也可以在内部直接连接。如果需要在外部进行信号处理的话,在程序设计的时候需要对config0寄存器bit4位置为1(默认值为0)。数据手册上给出了两种外部信号处理的电路,在数据手册的42和43页。
2、在程序设计的时候,数据手册上给出了一个流程(在数据手册的40页)。具体为:1)reset spi接口。这是非常重要的一步,这也是我调试花的时间最多地方。如果要使芯片能正常工作,首先要使spi能正常工作。在调试前,有必要仔细研究一下spi的时序(数据手册第7页,图1)。复位的步骤是先将cs置高一段时间再拉低,至于置高的时间我也没搞懂,如果按照数据手册上的4096个fclk的话,发现spi的输出线上的数据是乱的,然后我就不断地增加延长的时间,直至spi出现的数据与预想的差不多。sck的信号通过spi master端(可以是单片机、dsp、cpld/fpga等)给出,这里要注意sck的信号是需要的时候再给,而不是一直给的。比如在发送命令、读取寄存器值,或者读取数据的时候。当然,对另外一个管脚cs的控制也很重要,cs的控制也是在需要的时候再拉低,闲时置高。2)把start管脚置为0,停止转换。一般在初始化的时候基本上都是start=0的。3)软件复位芯片。有的是把reset脚通过硬件复位的,由于我们是软件复位的,不熟悉硬件复位的情况,所以对于硬件复位的话,这步可能不需要。4)配置寄存器。配置的值按照数据手册上的说明结合自己的实际需求给出。5)回读寄存器的值。这个步骤在调试的时候很有用,可以作为判断是否正常工作,如果读出来的值与写进去的值一样,说明spi能够正常工作,尤其是可以根据id寄存器的值来判断,因为这个值是固定的。当然,如果程序调试好了,这部分的程序是可以不要的。6)以上的步骤完成后,可以将start置为1,开始转换。7)开始读数据,读的方式按照数据手册上的三种(直接读,命令读,脉冲读)选一种即可,我选的是直接读,根据drdy的管脚来判断。基本上按照以上的流程来操作是没有问题的,不管是基于什么语言开发。在这里再次强调一下首先要保证spi能够正常通讯。
3、ads1258基本上和1158操作流程是一样的。网上关于1258的例程比1158的多。TI的这两款芯片用好了是高性能ad转换器,用不好能把人折腾死。数据手册一定要细读。我在调试期间在社区里发了两个帖子都烂尾,不知道是我问的问题太简单,还是工作人员太忙,最后也就不了了之。
4、以下是基于verilog编写的源代码。cpld的晶振是50M。分频后得到500K作为sck。
module adc(
clk,
rst_n,
cs,
sck,
start,
pwdn,
drdy,
miso,
mosi,
rst_ad,
dataout,
clkout
);
input clk,rst_n;
input miso; //from ad device
input drdy;
output reg start;
output reg rst_ad;
output reg pwdn;
output reg cs;
output sck;
output reg mosi ;//to ad device
reg[15:0] cnt;
output reg clkout;
always @(posedge clk or negedge rst_n)begin
if (!rst_n) begin
clkout <= 1'd0;
cnt<=16'd0;
end
else if (cnt == 16'd50) begin
clkout <=~clkout;
cnt <=16'd0;
end
else begin
cnt <=cnt+1'd1;
end
end
assign sck =clkout && flag_sck;//通过一个标志位与clkout与操作后得到sck
reg flag_sck;
reg [15:0]state_spi;
reg [31:0]time_delay1,time_delay2;
always @(negedge clkout or negedge rst_n) begin
if(!rst_n) begin
cs <=1'd1;
flag_sck <=1'd0;
rst_ad <=1'd0;
pwdn<=1'd1;
rst_ad<=1'd1;
state_spi<=16'd0;
time_delay1<=32'd0;
time_delay2<=32'd0;
end
else begin
case (state_spi)
16'd0: begin
cs<=1'd1;
flag_sck<=1'd0;
//start<=1'd0;
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd1: begin
if(time_delay1==32'd3000)begin //3000这个值是最后试出来的,如果按照500K的sck来算,远大于数据手册上的4096fclk。
cs<=1'd0;
flag_sck<=1'd1;
time_delay1<=32'd0;
state_spi<=state_spi+1'd1;
end
else begin
cs<=1'd1;
time_delay1<=time_delay1+1'd1;
end
end
16'd2: begin
start<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd3: begin
if(time_delay2==32'd3000)begin //复位芯片,这个值也是最后试出来的。
rst_ad<=1'd1;
time_delay2<=32'd0;
state_spi<=state_spi+1'd1;
end
else begin
rst_ad<=1'd0;
time_delay2<=time_delay2+1'd1;
end
end
16'd4: begin cs <=1'd1;flag_sck<=1'd0; state_spi<=state_spi+1'd1;end
16'd5: state_spi<=state_spi+1'd1;
16'd6: state_spi<=state_spi+1'd1;
16'd7: state_spi<=state_spi+1'd1;
16'd8: state_spi<=state_spi+1'd1;
16'd9: state_spi<=state_spi+1'd1;
16'd10: state_spi<=state_spi+1'd1;
16'd11: state_spi<=state_spi+1'd1;
16'd12: state_spi<=state_spi+1'd1;
16'd13: state_spi<=state_spi+1'd1;
16'd14: state_spi<=state_spi+1'd1;
16'd15: state_spi<=state_spi+1'd1;
16'd16: state_spi<=state_spi+1'd1;
16'd17: state_spi<=state_spi+1'd1;
16'd18: state_spi<=state_spi+1'd1;
16'd19: state_spi<=state_spi+1'd1;
16'd20: state_spi<=state_spi+1'd1;
16'd21: state_spi<=state_spi+1'd1;
16'd22: state_spi<=state_spi+1'd1;
16'd23: state_spi<=state_spi+1'd1;
16'd24: state_spi<=state_spi+1'd1;
16'd25: state_spi<=state_spi+1'd1;
16'd26: state_spi<=state_spi+1'd1;
16'd27: state_spi<=state_spi+1'd1;
16'd28: state_spi<=state_spi+1'd1;
16'd29: state_spi<=state_spi+1'd1;
16'd30: begin state_spi<=state_spi+1'd1; end
16'd31: begin
cs<=1'd0;
//flag_sck<=1'd1;
state_spi<=state_spi+1'd1;
end
//write register command
16'd32: begin
flag_sck<=1'd1;
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd33: begin
//flag_sck<=1'd1;
mosi<=1'd1;
state_spi<=state_spi+1'd1;
end
16'd34: begin
mosi<=1'd1;
state_spi<=state_spi+1'd1;
end
16'd35: begin
mosi<=1'd1;
state_spi<=state_spi+1'd1;
end
16'd36: begin
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd37: begin
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd38: begin
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
16'd39: begin
mosi<=1'd0;
state_spi<=state_spi+1'd1;
end
//config0
16'd40: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd41: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd42: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd43: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd44: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd45: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd46: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd47: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//config1
16'd48: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd49: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd50: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd51: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd52: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd53: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd54: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd55: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//muxsch
16'd56: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd57: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd58: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd59: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd60: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd61: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd62: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd63: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//muxdif
16'd64: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd65: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd66: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd67: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd68: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd69: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd70: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd71: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//muxsg0
16'd72: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd73: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd74: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end //
16'd75: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd76: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd77: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd78: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd79: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//muxsg1
16'd80: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd81: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd82: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end //
16'd83: begin //ch12
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd84: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd85: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd86: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd87: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//sysred
16'd88: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd89: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd90: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd91: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd92: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd93: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd94: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd95: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//gpioc
16'd96: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd97: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd98: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end //
16'd99: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd100: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd101: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd102: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd103: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//gpiod
16'd104: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd105: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd106: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end //
16'd107: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd108: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd109: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd110: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd111: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
//id
16'd112: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd113: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd114: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd115: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd116: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd117: begin
mosi <=1'd0;
state_spi<=state_spi+1'd1;
end
16'd118: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd119: begin
mosi <=1'd1;
state_spi<=state_spi+1'd1;
end
16'd120: begin
cs<=1'd1;
flag_sck<=1'd0;
mosi<=1'd0;
//start<=1'd1;
state_spi<=state_spi+1'd1;
end
16'd121:state_spi<=state_spi+1'd1;
16'd122:state_spi<=state_spi+1'd1;
16'd123:state_spi<=state_spi+1'd1;
16'd124:state_spi<=state_spi+1'd1;
16'd125:state_spi<=state_spi+1'd1;
16'd126:state_spi<=state_spi+1'd1;
16'd127:state_spi<=state_spi+1'd1;
16'd128:begin state_spi<=state_spi+1'd1;end
16'd129: begin cs<=1'd0;state_spi<=state_spi+1'd1;end
16'd130: begin flag_sck<=1'd1;mosi<=1'd0;state_spi<=state_spi+1'd1;end
16'd131: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end
16'd132: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd133: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end
16'd134: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd135: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd136: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd137: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd138: begin state_spi<=state_spi+1'd1;end
16'd139:begin state_spi<=state_spi+1'd1;end
16'd140:state_spi<=state_spi+1'd1;
16'd141:state_spi<=state_spi+1'd1;
16'd142:state_spi<=state_spi+1'd1;
16'd143:state_spi<=state_spi+1'd1;
16'd144:state_spi<=state_spi+1'd1;
16'd145:state_spi<=state_spi+1'd1;
16'd146:state_spi<=state_spi+1'd1;
16'd147:state_spi<=state_spi+1'd1;
16'd148:state_spi<=state_spi+1'd1;
16'd149:state_spi<=state_spi+1'd1;
16'd150:state_spi<=state_spi+1'd1;
16'd151:state_spi<=state_spi+1'd1;
16'd152:state_spi<=state_spi+1'd1;
16'd153:state_spi<=state_spi+1'd1;//16
16'd154: begin state_spi<=state_spi+1'd1;end
16'd155:state_spi<=state_spi+1'd1;
16'd156:state_spi<=state_spi+1'd1;
16'd157:state_spi<=state_spi+1'd1;
16'd158:state_spi<=state_spi+1'd1;
16'd159:state_spi<=state_spi+1'd1;
16'd160:state_spi<=state_spi+1'd1;
16'd161:state_spi<=state_spi+1'd1;
16'd162:state_spi<=state_spi+1'd1;
16'd163:state_spi<=state_spi+1'd1;
16'd164:state_spi<=state_spi+1'd1;
16'd165:state_spi<=state_spi+1'd1;
16'd166:state_spi<=state_spi+1'd1;
16'd167:state_spi<=state_spi+1'd1;
16'd168:state_spi<=state_spi+1'd1;
16'd169:state_spi<=state_spi+1'd1;
16'd170: begin state_spi<=state_spi+1'd1;end
16'd171:state_spi<=state_spi+1'd1;
16'd172:state_spi<=state_spi+1'd1;
16'd173:state_spi<=state_spi+1'd1;
16'd174:state_spi<=state_spi+1'd1;
16'd175:state_spi<=state_spi+1'd1;
16'd176:state_spi<=state_spi+1'd1;
16'd177:state_spi<=state_spi+1'd1;//40
16'd178:state_spi<=state_spi+1'd1;
16'd179:state_spi<=state_spi+1'd1;
16'd180:state_spi<=state_spi+1'd1;
16'd181:state_spi<=state_spi+1'd1;
16'd182:state_spi<=state_spi+1'd1;
16'd183:state_spi<=state_spi+1'd1;
16'd184:state_spi<=state_spi+1'd1;
16'd185:state_spi<=state_spi+1'd1;
16'd186: begin state_spi<=state_spi+1'd1;end
16'd187:state_spi<=state_spi+1'd1;
16'd188:state_spi<=state_spi+1'd1;
16'd189:state_spi<=state_spi+1'd1;
16'd190:state_spi<=state_spi+1'd1;
16'd191:state_spi<=state_spi+1'd1;
16'd192:state_spi<=state_spi+1'd1;
16'd193:state_spi<=state_spi+1'd1;
16'd194:state_spi<=state_spi+1'd1;
16'd195:state_spi<=state_spi+1'd1;
16'd196:state_spi<=state_spi+1'd1;
16'd197:state_spi<=state_spi+1'd1;
16'd198:state_spi<=state_spi+1'd1;
16'd199:state_spi<=state_spi+1'd1;
16'd200:state_spi<=state_spi+1'd1;
16'd201:state_spi<=state_spi+1'd1;
16'd202: begin state_spi<=state_spi+1'd1;end
16'd203:state_spi<=state_spi+1'd1;//66
16'd204:state_spi<=state_spi+1'd1;
16'd205:state_spi<=state_spi+1'd1;
16'd206:state_spi<=state_spi+1'd1;
16'd207:state_spi<=state_spi+1'd1;
16'd208:state_spi<=state_spi+1'd1;
16'd209:state_spi<=state_spi+1'd1;
16'd210:state_spi<=state_spi+1'd1;
16'd211:state_spi<=state_spi+1'd1;
16'd212:state_spi<=state_spi+1'd1;
16'd213:state_spi<=state_spi+1'd1;
16'd214:state_spi<=state_spi+1'd1;
16'd215:state_spi<=state_spi+1'd1;
16'd216:state_spi<=state_spi+1'd1;
16'd217:state_spi<=state_spi+1'd1;//88
16'd218:state_spi<=state_spi+1'd1;
16'd219:state_spi<=state_spi+1'd1;
16'd220:state_spi<=state_spi+1'd1;
16'd221:state_spi<=state_spi+1'd1;
16'd222:state_spi<=state_spi+1'd1;
16'd223:state_spi<=state_spi+1'd1;
16'd224:state_spi<=state_spi+1'd1;
16'd225:state_spi<=state_spi+1'd1;
16'd226:state_spi<=state_spi+1'd1;
16'd227: begin
cs<=1'd1;
flag_sck<=1'd0;
start<=1'd1;
state_spi<=state_spi+1'd1;//state_spi<=16'd228;
end
16'd228:state_spi<=state_spi+1'd1;
16'd229:state_spi<=state_spi+1'd1;
16'd230:state_spi<=state_spi+1'd1;
16'd231:state_spi<=state_spi+1'd1;
16'd232:state_spi<=state_spi+1'd1;
16'd233:state_spi<=state_spi+1'd1;
16'd234:state_spi<=state_spi+1'd1;
//16'd235:begin state_spi<=state_spi+1'd1;end
16'd235: begin
if(drdy==1'd0)begin
//cs<=1'd0;
state_spi<=state_spi+1'd1;
end
end
16'd236:begin cs<=1'd0;state_spi<=state_spi+1'd1;end
16'd237: begin flag_sck<=1'd1; mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd238: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd239: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd240: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd241: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd242: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd243: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd244: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end
16'd245: begin state_spi<=state_spi+1'd1;end
16'd246:state_spi<=state_spi+1'd1;
16'd247:state_spi<=state_spi+1'd1;
16'd248:state_spi<=state_spi+1'd1;
16'd249:state_spi<=state_spi+1'd1;
16'd250:state_spi<=state_spi+1'd1;
16'd251:state_spi<=state_spi+1'd1;
16'd252:state_spi<=state_spi+1'd1;
16'd253:state_spi<=state_spi+1'd1;
16'd254:state_spi<=state_spi+1'd1;
16'd255:state_spi<=state_spi+1'd1;
16'd256:state_spi<=state_spi+1'd1;
16'd257:state_spi<=state_spi+1'd1;
16'd258:state_spi<=state_spi+1'd1;
16'd259:state_spi<=state_spi+1'd1;
16'd260:state_spi<=state_spi+1'd1;
/*16'd261:state_spi<=state_spi+1'd1;
16'd262:state_spi<=state_spi+1'd1;
16'd263:state_spi<=state_spi+1'd1;
16'd264:state_spi<=state_spi+1'd1;
16'd265:state_spi<=state_spi+1'd1;
16'd266:state_spi<=state_spi+1'd1;
16'd267:state_spi<=state_spi+1'd1;
16'd268:state_spi<=state_spi+1'd1;
/*16'd154:state_spi<=state_spi+1'd1;
16'd155:state_spi<=state_spi+1'd1;
16'd156:state_spi<=state_spi+1'd1;
16'd157:state_spi<=state_spi+1'd1;
16'd158:state_spi<=state_spi+1'd1;
16'd159:state_spi<=state_spi+1'd1;
16'd160:state_spi<=state_spi+1'd1;
16'd161:state_spi<=state_spi+1'd1;*/
16'd261: begin
cs<=1'd1;
flag_sck<=1'd0;
flag_rdat<=1'd0;
state_spi<=16'd228;
end
default:state_spi<=16'd0;
endcase
end
end
endmodule