近期一直在调试ads1158,终于能够得到正常的输出,期间在网上查了很多的资料,发现关于ads1158的资料很少,尤其是基于verilog的程序几乎没有,所查的资料大多语焉不详,因此,本着人人为我,我为人人的精神,现在把ads1158的调试心得写出来,希望能够帮助一些开发者,节省开发时间。
1、在开发初期,由于是中途接手的项目,对硬件熟悉不够,导致耽误了不少时间,具体的硬件原因就不细说了,因为每一个开发者的硬件不可能是一样的,在这里给的建议是:在ads1158这部分的电路,可以根据数据手册来设计。另外,对于ads1158或者1258来说,模拟量是可以通过muxoutp(pin44)和muxoutn(pin43)引出来后自己添加一些信号处理的电路(如放大,滤波等),再由管脚adcinp(pin42)和adcinn(pin41)输入进芯片进行a/d转换,当然也可以在内部直接连接。如果需要在外部进行信号处理的话,在程序设计的时候需要对config0寄存器bit4位置为1(默认值为0)。数据手册上给出了两种外部信号处理的电路,在数据手册的42和43页。
2、在程序设计的时候,数据手册上给出了一个流程(在数据手册的40页)。具体为:1)reset spi接口。这是非常重要的一步,这也是我调试花的时间最多地方。如果要使芯片能正常工作,首先要使spi能正常工作。在调试前,有必要仔细研究一下spi的时序(数据手册第7页,图1)。复位的步骤是先将cs置高一段时间再拉低,至于置高的时间我也没搞懂,如果按照数据手册上的4096个fclk的话,发现spi的输出线上的数据是乱的,然后我就不断地增加延长的时间,直至spi出现的数据与预想的差不多。sck的信号通过spi master端(可以是单片机、dsp、cpld/fpga等)给出,这里要注意sck的信号是需要的时候再给,而不是一直给的。比如在发送命令、读取寄存器值,或者读取数据的时候。当然,对另外一个管脚cs的控制也很重要,cs的控制也是在需要的时候再拉低,闲时置高。2)把start管脚置为0,停止转换。一般在初始化的时候基本上都是start=0的。3)软件复位芯片。有的是把reset脚通过硬件复位的,由于我们是软件复位的,不熟悉硬件复位的情况,所以对于硬件复位的话,这步可能不需要。4)配置寄存器。配置的值按照数据手册上的说明结合自己的实际需求给出。5)回读寄存器的值。这个步骤在调试的时候很有用,可以作为判断是否正常工作,如果读出来的值与写进去的值一样,说明spi能够正常工作,尤其是可以根据id寄存器的值来判断,因为这个值是固定的。当然,如果程序调试好了,这部分的程序是可以不要的。6)以上的步骤完成后,可以将start置为1,开始转换。7)开始读数据,读的方式按照数据手册上的三种(直接读,命令读,脉冲读)选一种即可,我选的是直接读,根据drdy的管脚来判断。基本上按照以上的流程来操作是没有问题的,不管是基于什么语言开发。在这里再次强调一下首先要保证spi能够正常通讯。
3、ads1258基本上和1158操作流程是一样的。网上关于1258的例程比1158的多。TI的这两款芯片用好了是高性能ad转换器,用不好能把人折腾死。数据手册一定要细读。我在调试期间在社区里发了两个帖子都烂尾,不知道是我问的问题太简单,还是工作人员太忙,最后也就不了了之。
4、以下是基于verilog编写的源代码。cpld的晶振是50M。分频后得到500K作为sck。
module adc( clk, rst_n, cs, sck, start, pwdn, drdy, miso, mosi, rst_ad, dataout, clkout ); input clk,rst_n; input miso; //from ad device input drdy; output reg start; output reg rst_ad; output reg pwdn; output reg cs; output sck; output reg mosi ;//to ad device reg[15:0] cnt; output reg clkout; always @(posedge clk or negedge rst_n)begin if (!rst_n) begin clkout <= 1'd0; cnt<=16'd0; end else if (cnt == 16'd50) begin clkout <=~clkout; cnt <=16'd0; end else begin cnt <=cnt+1'd1; end end assign sck =clkout && flag_sck;//通过一个标志位与clkout与操作后得到sck reg flag_sck; reg [15:0]state_spi; reg [31:0]time_delay1,time_delay2; always @(negedge clkout or negedge rst_n) begin if(!rst_n) begin cs <=1'd1; flag_sck <=1'd0; rst_ad <=1'd0; pwdn<=1'd1; rst_ad<=1'd1; state_spi<=16'd0; time_delay1<=32'd0; time_delay2<=32'd0; end else begin case (state_spi) 16'd0: begin cs<=1'd1; flag_sck<=1'd0; //start<=1'd0; mosi<=1'd0; state_spi<=state_spi+1'd1; end 16'd1: begin if(time_delay1==32'd3000)begin //3000这个值是最后试出来的,如果按照500K的sck来算,远大于数据手册上的4096fclk。 cs<=1'd0; flag_sck<=1'd1; time_delay1<=32'd0; state_spi<=state_spi+1'd1; end else begin cs<=1'd1; time_delay1<=time_delay1+1'd1; end end 16'd2: begin start<=1'd0; state_spi<=state_spi+1'd1; end 16'd3: begin if(time_delay2==32'd3000)begin //复位芯片,这个值也是最后试出来的。 rst_ad<=1'd1; time_delay2<=32'd0; state_spi<=state_spi+1'd1; end else begin rst_ad<=1'd0; time_delay2<=time_delay2+1'd1; end end 16'd4: begin cs <=1'd1;flag_sck<=1'd0; state_spi<=state_spi+1'd1;end 16'd5: state_spi<=state_spi+1'd1; 16'd6: state_spi<=state_spi+1'd1; 16'd7: state_spi<=state_spi+1'd1; 16'd8: state_spi<=state_spi+1'd1; 16'd9: state_spi<=state_spi+1'd1; 16'd10: state_spi<=state_spi+1'd1; 16'd11: state_spi<=state_spi+1'd1; 16'd12: state_spi<=state_spi+1'd1; 16'd13: state_spi<=state_spi+1'd1; 16'd14: state_spi<=state_spi+1'd1; 16'd15: state_spi<=state_spi+1'd1; 16'd16: state_spi<=state_spi+1'd1; 16'd17: state_spi<=state_spi+1'd1; 16'd18: state_spi<=state_spi+1'd1; 16'd19: state_spi<=state_spi+1'd1; 16'd20: state_spi<=state_spi+1'd1; 16'd21: state_spi<=state_spi+1'd1; 16'd22: state_spi<=state_spi+1'd1; 16'd23: state_spi<=state_spi+1'd1; 16'd24: state_spi<=state_spi+1'd1; 16'd25: state_spi<=state_spi+1'd1; 16'd26: state_spi<=state_spi+1'd1; 16'd27: state_spi<=state_spi+1'd1; 16'd28: state_spi<=state_spi+1'd1; 16'd29: state_spi<=state_spi+1'd1; 16'd30: begin state_spi<=state_spi+1'd1; end 16'd31: begin cs<=1'd0; //flag_sck<=1'd1; state_spi<=state_spi+1'd1; end //write register command 16'd32: begin flag_sck<=1'd1; mosi<=1'd0; state_spi<=state_spi+1'd1; end 16'd33: begin //flag_sck<=1'd1; mosi<=1'd1; state_spi<=state_spi+1'd1; end 16'd34: begin mosi<=1'd1; state_spi<=state_spi+1'd1; end 16'd35: begin mosi<=1'd1; state_spi<=state_spi+1'd1; end 16'd36: begin mosi<=1'd0; state_spi<=state_spi+1'd1; end 16'd37: begin mosi<=1'd0; state_spi<=state_spi+1'd1; end 16'd38: begin mosi<=1'd0; state_spi<=state_spi+1'd1; end 16'd39: begin mosi<=1'd0; state_spi<=state_spi+1'd1; end //config0 16'd40: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd41: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd42: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd43: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd44: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd45: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd46: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd47: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //config1 16'd48: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd49: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd50: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd51: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd52: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd53: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd54: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd55: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //muxsch 16'd56: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd57: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd58: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd59: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd60: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd61: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd62: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd63: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //muxdif 16'd64: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd65: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd66: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd67: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd68: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd69: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd70: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd71: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //muxsg0 16'd72: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd73: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd74: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end // 16'd75: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd76: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd77: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd78: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd79: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //muxsg1 16'd80: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd81: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd82: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end // 16'd83: begin //ch12 mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd84: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd85: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd86: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd87: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //sysred 16'd88: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd89: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd90: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd91: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd92: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd93: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd94: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd95: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //gpioc 16'd96: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd97: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd98: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end // 16'd99: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd100: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd101: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd102: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd103: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //gpiod 16'd104: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd105: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd106: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end // 16'd107: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd108: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd109: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd110: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd111: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end //id 16'd112: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd113: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd114: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd115: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd116: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd117: begin mosi <=1'd0; state_spi<=state_spi+1'd1; end 16'd118: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd119: begin mosi <=1'd1; state_spi<=state_spi+1'd1; end 16'd120: begin cs<=1'd1; flag_sck<=1'd0; mosi<=1'd0; //start<=1'd1; state_spi<=state_spi+1'd1; end 16'd121:state_spi<=state_spi+1'd1; 16'd122:state_spi<=state_spi+1'd1; 16'd123:state_spi<=state_spi+1'd1; 16'd124:state_spi<=state_spi+1'd1; 16'd125:state_spi<=state_spi+1'd1; 16'd126:state_spi<=state_spi+1'd1; 16'd127:state_spi<=state_spi+1'd1; 16'd128:begin state_spi<=state_spi+1'd1;end 16'd129: begin cs<=1'd0;state_spi<=state_spi+1'd1;end 16'd130: begin flag_sck<=1'd1;mosi<=1'd0;state_spi<=state_spi+1'd1;end 16'd131: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end 16'd132: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd133: begin mosi<=1'd1; state_spi<=state_spi+1'd1;end 16'd134: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd135: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd136: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd137: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd138: begin state_spi<=state_spi+1'd1;end 16'd139:begin state_spi<=state_spi+1'd1;end 16'd140:state_spi<=state_spi+1'd1; 16'd141:state_spi<=state_spi+1'd1; 16'd142:state_spi<=state_spi+1'd1; 16'd143:state_spi<=state_spi+1'd1; 16'd144:state_spi<=state_spi+1'd1; 16'd145:state_spi<=state_spi+1'd1; 16'd146:state_spi<=state_spi+1'd1; 16'd147:state_spi<=state_spi+1'd1; 16'd148:state_spi<=state_spi+1'd1; 16'd149:state_spi<=state_spi+1'd1; 16'd150:state_spi<=state_spi+1'd1; 16'd151:state_spi<=state_spi+1'd1; 16'd152:state_spi<=state_spi+1'd1; 16'd153:state_spi<=state_spi+1'd1;//16 16'd154: begin state_spi<=state_spi+1'd1;end 16'd155:state_spi<=state_spi+1'd1; 16'd156:state_spi<=state_spi+1'd1; 16'd157:state_spi<=state_spi+1'd1; 16'd158:state_spi<=state_spi+1'd1; 16'd159:state_spi<=state_spi+1'd1; 16'd160:state_spi<=state_spi+1'd1; 16'd161:state_spi<=state_spi+1'd1; 16'd162:state_spi<=state_spi+1'd1; 16'd163:state_spi<=state_spi+1'd1; 16'd164:state_spi<=state_spi+1'd1; 16'd165:state_spi<=state_spi+1'd1; 16'd166:state_spi<=state_spi+1'd1; 16'd167:state_spi<=state_spi+1'd1; 16'd168:state_spi<=state_spi+1'd1; 16'd169:state_spi<=state_spi+1'd1; 16'd170: begin state_spi<=state_spi+1'd1;end 16'd171:state_spi<=state_spi+1'd1; 16'd172:state_spi<=state_spi+1'd1; 16'd173:state_spi<=state_spi+1'd1; 16'd174:state_spi<=state_spi+1'd1; 16'd175:state_spi<=state_spi+1'd1; 16'd176:state_spi<=state_spi+1'd1; 16'd177:state_spi<=state_spi+1'd1;//40 16'd178:state_spi<=state_spi+1'd1; 16'd179:state_spi<=state_spi+1'd1; 16'd180:state_spi<=state_spi+1'd1; 16'd181:state_spi<=state_spi+1'd1; 16'd182:state_spi<=state_spi+1'd1; 16'd183:state_spi<=state_spi+1'd1; 16'd184:state_spi<=state_spi+1'd1; 16'd185:state_spi<=state_spi+1'd1; 16'd186: begin state_spi<=state_spi+1'd1;end 16'd187:state_spi<=state_spi+1'd1; 16'd188:state_spi<=state_spi+1'd1; 16'd189:state_spi<=state_spi+1'd1; 16'd190:state_spi<=state_spi+1'd1; 16'd191:state_spi<=state_spi+1'd1; 16'd192:state_spi<=state_spi+1'd1; 16'd193:state_spi<=state_spi+1'd1; 16'd194:state_spi<=state_spi+1'd1; 16'd195:state_spi<=state_spi+1'd1; 16'd196:state_spi<=state_spi+1'd1; 16'd197:state_spi<=state_spi+1'd1; 16'd198:state_spi<=state_spi+1'd1; 16'd199:state_spi<=state_spi+1'd1; 16'd200:state_spi<=state_spi+1'd1; 16'd201:state_spi<=state_spi+1'd1; 16'd202: begin state_spi<=state_spi+1'd1;end 16'd203:state_spi<=state_spi+1'd1;//66 16'd204:state_spi<=state_spi+1'd1; 16'd205:state_spi<=state_spi+1'd1; 16'd206:state_spi<=state_spi+1'd1; 16'd207:state_spi<=state_spi+1'd1; 16'd208:state_spi<=state_spi+1'd1; 16'd209:state_spi<=state_spi+1'd1; 16'd210:state_spi<=state_spi+1'd1; 16'd211:state_spi<=state_spi+1'd1; 16'd212:state_spi<=state_spi+1'd1; 16'd213:state_spi<=state_spi+1'd1; 16'd214:state_spi<=state_spi+1'd1; 16'd215:state_spi<=state_spi+1'd1; 16'd216:state_spi<=state_spi+1'd1; 16'd217:state_spi<=state_spi+1'd1;//88 16'd218:state_spi<=state_spi+1'd1; 16'd219:state_spi<=state_spi+1'd1; 16'd220:state_spi<=state_spi+1'd1; 16'd221:state_spi<=state_spi+1'd1; 16'd222:state_spi<=state_spi+1'd1; 16'd223:state_spi<=state_spi+1'd1; 16'd224:state_spi<=state_spi+1'd1; 16'd225:state_spi<=state_spi+1'd1; 16'd226:state_spi<=state_spi+1'd1; 16'd227: begin cs<=1'd1; flag_sck<=1'd0; start<=1'd1; state_spi<=state_spi+1'd1;//state_spi<=16'd228; end 16'd228:state_spi<=state_spi+1'd1; 16'd229:state_spi<=state_spi+1'd1; 16'd230:state_spi<=state_spi+1'd1; 16'd231:state_spi<=state_spi+1'd1; 16'd232:state_spi<=state_spi+1'd1; 16'd233:state_spi<=state_spi+1'd1; 16'd234:state_spi<=state_spi+1'd1; //16'd235:begin state_spi<=state_spi+1'd1;end 16'd235: begin if(drdy==1'd0)begin //cs<=1'd0; state_spi<=state_spi+1'd1; end end 16'd236:begin cs<=1'd0;state_spi<=state_spi+1'd1;end 16'd237: begin flag_sck<=1'd1; mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd238: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd239: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd240: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd241: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd242: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd243: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd244: begin mosi<=1'd0; state_spi<=state_spi+1'd1;end 16'd245: begin state_spi<=state_spi+1'd1;end 16'd246:state_spi<=state_spi+1'd1; 16'd247:state_spi<=state_spi+1'd1; 16'd248:state_spi<=state_spi+1'd1; 16'd249:state_spi<=state_spi+1'd1; 16'd250:state_spi<=state_spi+1'd1; 16'd251:state_spi<=state_spi+1'd1; 16'd252:state_spi<=state_spi+1'd1; 16'd253:state_spi<=state_spi+1'd1; 16'd254:state_spi<=state_spi+1'd1; 16'd255:state_spi<=state_spi+1'd1; 16'd256:state_spi<=state_spi+1'd1; 16'd257:state_spi<=state_spi+1'd1; 16'd258:state_spi<=state_spi+1'd1; 16'd259:state_spi<=state_spi+1'd1; 16'd260:state_spi<=state_spi+1'd1; /*16'd261:state_spi<=state_spi+1'd1; 16'd262:state_spi<=state_spi+1'd1; 16'd263:state_spi<=state_spi+1'd1; 16'd264:state_spi<=state_spi+1'd1; 16'd265:state_spi<=state_spi+1'd1; 16'd266:state_spi<=state_spi+1'd1; 16'd267:state_spi<=state_spi+1'd1; 16'd268:state_spi<=state_spi+1'd1; /*16'd154:state_spi<=state_spi+1'd1; 16'd155:state_spi<=state_spi+1'd1; 16'd156:state_spi<=state_spi+1'd1; 16'd157:state_spi<=state_spi+1'd1; 16'd158:state_spi<=state_spi+1'd1; 16'd159:state_spi<=state_spi+1'd1; 16'd160:state_spi<=state_spi+1'd1; 16'd161:state_spi<=state_spi+1'd1;*/ 16'd261: begin cs<=1'd1; flag_sck<=1'd0; flag_rdat<=1'd0; state_spi<=16'd228; end default:state_spi<=16'd0; endcase end end
endmodule