This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC09QJ1300: 子类1模式输出可以建链,但是数据为乱码

Part Number: ADC09QJ1300


ADC09QJ1300的CLK给了100M时钟,SYSREF给了7.8125M,FPGA的GLBLCLK及REFCLK均为125M,SYSREF为7.8125M。

在使用ADC的测试模式时,JESD204BIP核中的输出信号为乱码。

ARM软核的配置代码在附件中,请麻烦帮忙检查一下是否有问题。

#include "xparameters.h"
#include "sleep.h"
#include "xgpio.h"
#include "xil_io.h"
#include "xil_types.h"
//#include <stdio.h>
//#include <stdlib.h>
/*	// spi的地址和数据

	6'h00:      rdata = { 31'b0 , spi_busy      };
	6'h01:      rdata = { 8'b0  , spi_wr_data   };
	6'h02:      rdata = { 24'b0 , spi_rd_data   };
*/


XGpio LMK_CFG;
#define LMK_BASE_ADDR 0x44A10000
#define ADC_BASE_ADDR 0x44A00000
#define R_JESD_BADDR  0x44A20000


u32 LMK_DATA[136] = {

		0x000090,	0x000010,	0x000200,	0x000306,	0x0004D0,	0x00055B,	0x000600,	0x000C51,
		0x000D04,	0x01001E,	0x010155,	0x010255,	0x010300,	0x010422,	0x010500,	0x0106F0,
		0x010755,	0x01081E,	0x010955,	0x010A55,	0x010B00,	0x010C22,	0x010D00,	0x010EF0,
		0x010F55,	0x011018,	0x011155,	0x011255,	0x011300,	0x011402,	0x011500,	0x0116F1,
		0x011705,	0x011818,	0x011955,	0x011A55,	0x011B00,	0x011C02,	0x011D00,	0x011EF1,
		0x011F05,	0x01200C,	0x012155,	0x012255,	0x012300,	0x012402,	0x012500,	0x0126F1,
		0x012705,	0x01280C,	0x012955,	0x012A55,	0x012B00,	0x012C02,	0x012D00,	0x012EF1,
		0x012F05,	0x013006,	0x013155,	0x013255,	0x013300,	0x013422,	0x013500,	0x0136F0,
		0x013750,	0x013825,	0x013903,	0x013A01,	0x013B80,	0x013C00,	0x013D08,	0x013E00,
		0x013F02,	0x014081,	0x014100,	0x014200,	0x014310,	0x0144FF,	0x01457F,	0x014619,
		0x014713,	0x014802,	0x014942,	0x014A33,	0x014B16,	0x014C00,	0x014D00,	0x014EC0,
		0x014F7F,	0x015003,	0x015102,	0x015200,	0x015300,	0x015473,	0x015500,	0x01560A,
		0x015700,	0x015896,	0x015900,	0x015A01,	0x015BD4,	0x015C20,	0x015D00,	0x015E00,
		0x015F0B,	0x016000,	0x016105,	0x016244,	0x016300,	0x016400,	0x01650C,	0x0171AA,
		0x017202,	0x017C15,	0x017D33,	0x016600,	0x016700,	0x016896,	0x016959,	0x016A20,
		0x016B00,	0x016C00,	0x016D00,	0x016E13,	0x017300,	0x018200,	0x018300,	0x018400,
		0x018500,	0x018800,	0x018900,	0x018A00,	0x018B00,	0x1FFD00,	0x1FFE00,	0x1FFF53

};

u32 DAC_CFG_DATA[102] = {

		0x000018, 0x010003, 0x022002, 0x03A300, 0x040000, 0x05FF03, 0x06FFFF, 0x073100,
		0x080000, 0x090000, 0x0A0000, 0x0B0000, 0x0C0400, 0x0D0400, 0x0E0400, 0x0F0400,
		0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000,
		0x180000, 0x190000, 0x1A0020, 0x1B0000, 0x1E9999, 0x1F9980, 0x208008, 0x221B1B,
		0x2301FF, 0x240020, 0x252000, 0x260000, 0x2D0001, 0x2EFFFF, 0x2F0004, 0x300000,
		0x311000, 0x320000, 0x330000, 0x340000, 0x3B0800, 0x3C0028, 0x3D0088, 0x3E0108,
		0x3F0000, 0x461882, 0x4701C8, 0x483143, 0x490000, 0x4AFF01, 0x4B1200, 0x4C1307,
		0x4D0300, 0x4E0F4F, 0x4F1C61, 0x500000, 0x5100DC, 0x5200FF, 0x530000, 0x5400FC,
		0x5500FF, 0x560000, 0x5700FF, 0x5800FF, 0x590000, 0x5A00FF, 0x5B00FF, 0x5C1133,
		0x5E0000, 0x5F3210, 0x605764, 0x610211, 0x640001, 0x650001, 0x660001, 0x670001,
		0x687709, 0x690000, 0x6A0000, 0x6BBD07, 0x6C0007, 0x6D0090, 0x6E0000, 0x6F0000,
		0x700000, 0x710000, 0x720000, 0x730000, 0x740000, 0x750000, 0x760000, 0x770000,
		0x780000, 0x790000, 0x7A0000, 0x7B0000, 0x7C0000, 0x7D0000

};

u32 Xil_SPI( u32 spi_addr, u32 dev_raddr){
	u32 rd_state = 0;
	u32 rd_data = 0;
	Xil_Out32(spi_addr + 0x04 , dev_raddr);				//写入读取数据的命令
	do{
		rd_state = Xil_In32(spi_addr + 0x0);	//读取忙状态
	}while(rd_state == 0x1);
	rd_data = Xil_In32(spi_addr + 0x8);		//读取读出数据
	//usleep(1);
	return rd_data;
}

int DAC_INIT(void){

}

int ADC_INIT(void){

	u32 Xil_Rdata = 0;

	Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x800C00); //读取FPGAVID

	Xil_SPI(ADC_BASE_ADDR , 0x0000B0); //AD芯片复位,等待750ns,地址0x00,默认数据0x30
	usleep(1000);
	//do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while(Xil_Rdata == 0x0);	//读取cpll锁定状态

	do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x827000); }while(Xil_Rdata == 0x0);	//读取init状态,直到返回1,在继续

	//Xil_SPI(ADC_BASE_ADDR , 0x002B05);	//设置参考时钟消抖

	Xil_SPI(ADC_BASE_ADDR , 0x002A03);
	Xil_SPI(ADC_BASE_ADDR , 0x0029B0);

	Xil_SPI(ADC_BASE_ADDR , 0x003F4A);	//向vco_bias中写入0x4a来设置vco的偏置
	Xil_SPI(ADC_BASE_ADDR , 0x005881);	//调整调整PLL输入管脚设置为管脚模式或者SPI模式,以及输入模式设置。
	Xil_SPI(ADC_BASE_ADDR , 0x005C01);	//编程cpll_reset置1到复位以继续cpll编程

	//Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x803F00);

	Xil_SPI(ADC_BASE_ADDR , 0x003D05);	//设置pll_p_div,pll_v_div,目前要求是1000M,根据手册可知,需要的p*v=8,在这里设置成p=2,v=4
	Xil_SPI(ADC_BASE_ADDR , 0x003E0A);	//设置pll_n_div 公式为:采样率 = N * Fref,因为在SE_CLK口输入的频率为100MHZ,则需要写入十进制的10,即16进制的0A,达到1000M频率	//***********************************
	Xil_SPI(ADC_BASE_ADDR , 0x005D41);	//设置vco_cal_en到1以启动vco校准
	Xil_SPI(ADC_BASE_ADDR , 0x005C00);	//设置将cpll设置到0以校准和启动vco及启动cpll

	Xil_SPI(ADC_BASE_ADDR , 0x005781);	//TRIGOUT输出控制

	Xil_SPI(ADC_BASE_ADDR , 0x002B15);

	usleep(1000);

	do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x805E00); }while(Xil_Rdata == 0x0);	//读取vco校准状态直到校准完成
	//GET_BIT();
	//do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while(Xil_Rdata == 0x0);	//读取CPLL校准状态直到校准完成(读到1)
	do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x820800); }while((Xil_Rdata << 31) != 0x80000000);	//读取CPLL校准状态直到校准完成(读到1)

	Xil_SPI(ADC_BASE_ADDR , 0x020000);	//关闭JESD204接口的状态机,以允许更改设置
	Xil_SPI(ADC_BASE_ADDR , 0x006100);	//关闭校准状态机以允许设置
	//Xil_SPI(ADC_BASE_ADDR , 0x003746);	//设置低功率模式1寄存器,设置1G及以内的低功率
	//Xil_SPI(ADC_BASE_ADDR , 0x029A06);	//设置低功率模式2寄存器,设置1G及以内的低功率
	//Xil_SPI(ADC_BASE_ADDR , 0x029B00);	//设置低功率模式3寄存器,设置1G及以内的低功率
	//Xil_SPI(ADC_BASE_ADDR , 0x029C14);	//设置低功率模式4寄存器,设置1G及以内的低功率

	Xil_SPI(ADC_BASE_ADDR , 0x020109);	//设置JMODE,选定的输出模式为JMODE1
	Xil_SPI(ADC_BASE_ADDR , 0x02021f);	//设置KM1寄存器,目前的值为默认的十进制的31,即十六进制的1F
	Xil_SPI(ADC_BASE_ADDR , 0x020401);	//选择同步信号是单端还是查分输入,此处选择默认单端

	Xil_SPI(ADC_BASE_ADDR , 0x020505);

	//Xil_SPI(ADC_BASE_ADDR , 0x006201);	//设置默认前景校准
	//Xil_SPI(ADC_BASE_ADDR , 0x006501);	//设置默认偏移参考值

	//Xil_SPI(ADC_BASE_ADDR , 0x005781);	//TRIGOUT输出控制

	Xil_SPI(ADC_BASE_ADDR , 0x02130f);	//启动超量程显示

	Xil_SPI(ADC_BASE_ADDR , 0x006101);	//启动校准状态机

	Xil_SPI(ADC_BASE_ADDR , 0x020001);	//启动jesd204的状态机

	Xil_SPI(ADC_BASE_ADDR , 0x006C00);	//拉低启动前景校准器的命令
	Xil_SPI(ADC_BASE_ADDR , 0x006C01);	//拉高启动前景校准器的命令
	do{ Xil_Rdata = Xil_SPI(ADC_BASE_ADDR , 0x806A00); }while(Xil_Rdata == 0x0);	//读取前景校准状态直到校准完成

	return 0;
}

int	RD_JESD_INIT(void){
	u32 Xil_Rdata = 0;
	Xil_Out32(R_JESD_BADDR + 0x08 , 0x01);	//启动ILA
	Xil_Out32(R_JESD_BADDR + 0x0C , 0x00);	//不加扰码
	Xil_Out32(R_JESD_BADDR + 0x10 , 0x01);	//掉链后自动重连
	Xil_Out32(R_JESD_BADDR + 0x18 , 0x00);	//测试模式选择普通模式
	Xil_Out32(R_JESD_BADDR + 0x20 , 0x00);	//设置F = 1
	Xil_Out32(R_JESD_BADDR + 0x24 , 0x1f);	//设置K =32
	Xil_Out32(R_JESD_BADDR + 0x28 , 0xff);	//设置全通道启动

	Xil_Out32(R_JESD_BADDR + 0x2C , 0x01);	//设置子类1
	//Xil_Out32(R_JESD_BADDR + 0x2C , 0x00);	//设置子类0

	Xil_Out32(R_JESD_BADDR + 0x30 , 0xfff);	//设置RX缓冲延时
	Xil_Out32(R_JESD_BADDR + 0x34 , 0x00);	//关闭错误计数,启动sync报错
	Xil_Out32(R_JESD_BADDR + 0x04 , 0x00010001);	//启动复位信号

	do{ Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x04); }while( Xil_Rdata != 0x00010000 );//等待RX的reset拉低(reset完成)
	do{ Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x38); }while( Xil_Rdata != 0x00010001 );//等待RX获得sync和连接

	/*
	while(1){
		usleep(1);
		//Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x04);	//复位状态
		Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x38);	//sync状态

		Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x1C);	//链接错误报警
		//Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x30);
		Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x34);	//错误报告
		Xil_Rdata = Xil_In32(R_JESD_BADDR + 0x824);
	}
	 */
	return 0;
}

int LMK_INIT(void){
	int	status;
	u32 Xil_Rdata = 0;

	/*
	do{ status	= XGpio_Initialize(&LMK_CFG  	,  	XPAR_GPIO_0_DEVICE_ID	);	}while( status != 0 );		//设置使能初始化

	XGpio_DiscreteWrite(&LMK_CFG,		1,		0x0);
	usleep(500);
	XGpio_DiscreteWrite(&LMK_CFG,		1,		0x1);
	usleep(1000);*/

	do{ status	= XGpio_Initialize(&LMK_CFG  	,  	XPAR_GPIO_0_DEVICE_ID	);	}while( status != 0 );		//设置使能初始化
	XGpio_DiscreteWrite(&LMK_CFG,		1,		0x1);

	Xil_SPI(LMK_BASE_ADDR , 0x000090);
	usleep(1000);
	Xil_SPI(LMK_BASE_ADDR , 0x000010);
	usleep(1000);

	XGpio_DiscreteWrite(&LMK_CFG,		1,		0x0);

	Xil_SPI(LMK_BASE_ADDR , 0x014A33);
	usleep(1000);

	Xil_Rdata = Xil_SPI(LMK_BASE_ADDR , 0x800400);	//读取PROD ID MSB
	Xil_Rdata = Xil_SPI(LMK_BASE_ADDR , 0x800500);	//读取PROD ID LSB

	int i = 0;
	for( i = 2; i <= 136; i++){
		Xil_SPI(LMK_BASE_ADDR , LMK_DATA[i]);
		usleep(1);
	}



	return 0;
}


int main(void) {
	//u32 Xil_Rdata = 0;

	usleep(1000);
	LMK_INIT();
	usleep(1000);

	ADC_INIT();
	RD_JESD_INIT();

	return 0;
}