你好,
最近使用TI的ADS8588S遇到如下问题:
如下图所示, 5V是AVDD、3.3V是DVDD、AD2V5_1和AD2V5_2分别是两片ADS8588S的REFIN/REFOUT管脚;
REFSEL外部配置都是10k上拉到3.3V,5V上电、3.3V还未上电过程中,一片直接输出2.5V,一片输出0V,3.3V上电后基准输出是和REFSEL配置一致的。
ADS8588S在5V上电3.3V还未上电的过程中,REFIN/REFOUT管脚的输出状态是不确定的吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
最近使用TI的ADS8588S遇到如下问题:
如下图所示, 5V是AVDD、3.3V是DVDD、AD2V5_1和AD2V5_2分别是两片ADS8588S的REFIN/REFOUT管脚;
REFSEL外部配置都是10k上拉到3.3V,5V上电、3.3V还未上电过程中,一片直接输出2.5V,一片输出0V,3.3V上电后基准输出是和REFSEL配置一致的。
ADS8588S在5V上电3.3V还未上电的过程中,REFIN/REFOUT管脚的输出状态是不确定的吗?

您好,
REFSEL是高电平才能使能内部参考电压输出,内部参考电压是AVDD产生的,按理说 AVDD和REFSEL同时满足要求了内部基准电压才有输出。
3.3V还未上电过程中,一片直接输出2.5V
我怀疑可能是这片 ADS8588S在上次上电掉电时,REFSEL管脚电压没有完全掉下来,使得AVDD有电时就有参考电压输出;另一个考虑是在3.3V还未上电时这片AD REFSEL管脚可能耦合了电磁干扰,干扰信号拉高了REFSEL管脚,使能了内部参考电压。
不知道3.3V还未上电的这片,与另一片电路图、PCB、外围器件使用物料等有没有区别?上电起始状态是否一样,是否存在有器件未完全放电状态?