This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8588S: ADS8588S上电时REFIN/REFOUT管脚输出问题

Part Number: ADS8588S


你好,

     最近使用TIADS8588S遇到如下问题:

      如下图所示, 5VAVDD3.3VDVDDAD2V5_1AD2V5_2分别是两片ADS8588SREFIN/REFOUT管脚;

      REFSEL外部配置都是10k上拉到3.3V5V上电、3.3V还未上电过程中,一片直接输出2.5V,一片输出0V3.3V上电后基准输出是和REFSEL配置一致的。

      ADS8588S5V上电3.3V还未上电的过程中,REFIN/REFOUT管脚的输出状态是不确定的吗?

  • 您好,

    REFSEL是高电平才能使能内部参考电压输出,内部参考电压是AVDD产生的,按理说 AVDD和REFSEL同时满足要求了内部基准电压才有输出。

    3.3V还未上电过程中,一片直接输出2.5V

    我怀疑可能是这片 ADS8588S在上次上电掉电时,REFSEL管脚电压没有完全掉下来,使得AVDD有电时就有参考电压输出;另一个考虑是在3.3V还未上电时这片AD REFSEL管脚可能耦合了电磁干扰,干扰信号拉高了REFSEL管脚,使能了内部参考电压。

    不知道3.3V还未上电的这片,与另一片电路图、PCB、外围器件使用物料等有没有区别?上电起始状态是否一样,是否存在有器件未完全放电状态?

  • 上电时,除了两种供电电压和参考输出电压,您可以同时测量两片芯片的REFSEL管脚的电压波形吗?我想看下“3.3V还未上电过程中,一片直接输出2.5V”,这片ADC的REFSEL管脚是否为高电平?如果是干扰造成的,那示波器探头测量此管脚时可能就不准了,因为不属于悬空状态了。