This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8830: 用FPGA以1us的间隔通过SPI协议给DAC8830一个16bit的数据点,使它分别产生一个100mV 30KHz和13KHz的正弦波,但是DAC8830输出的正弦波毛刺很大,请问这是为什么?

Part Number: DAC8830


DAC8830的原理图参照的是DAC8830评估板的原理图,DAC8830的5V电压用的是AMS1117-5供电:

因为我要最大输出500mV  35KHz的正弦波,所以我将DAC8830的Vout引脚接了一个电容C101 进行滤波,然后经过电压跟随器后再经过R69 , C93进行滤波。

但是我用示波器测试到C93两端的正弦波波形很大毛刺,因此我就直接用示波器测DAC8830的Vout引脚接的C101电容的波形,发现它们的毛刺都一模一样,下图是我测的DAC8830的Vout引脚的波形:

波形测量方式:

请问为什么DAC8830输出100mV正弦波的时候毛刺这么大?