请介绍一下ADS5474模数转换器的VCM和VREF引脚在什么情况下使用?
文档上说VCM是在直流耦合应用时用于设置共模电压,是不是指前级驱动电路使用放大器的时候?如果前面直接使用变压器耦合成差分输入是不是不能用VCM?另外,VCM引脚在芯片内部通过2个500欧电阻接到两个输入,既然在内部已经偏置了,为什么还要输出到外部去作共模电压?
文档上说VREF引脚既可用作输入又可用作输出,具体作用是什么?在什么情况下使用?文档上有张图表明两个时钟引脚在内部通过两个1000欧电阻接到2.4V电压,这个2.4V是不是就是VREF?
此外,信号输入规定是2.2VPP,共模电压设置为3.1V或是0V是不是都行?