This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: Vcap的電壓問題

Part Number: ADS1299


使用自製的PCB版,檢測輸入點電壓都沒問題,如圖1到圖3

圖1.(DVDD,3.3V)

圖2.(AVDD,2.5V)

圖3.(AVSS,-2.5V)


圖4.VCAP1

圖5.VCAP2

圖6.VCAP3

圖7.VCAP4

圖8.Vref


根據[FAQ] ADS1298: ADS129x:如何验证 ADS129x 器件是否仍然正常工作? ,檢測內部電壓節點,發現VCAPx 都有問題
ADS1299的 連接 VCAP1 的電容C22跨壓卻是0V,C22兩端皆為-2.5V,連接 VCAP2 的電容C23跨壓在-1~-0.3V之間來回,連接 VCAP3 的電容C18跨壓為4.07V,連接 VCAP4 的電容C19跨壓為1.1V,連接 Vref 的電容C14跨壓為0.07V
想請問可能的原因?