使用THS8200芯片,输入为3x8bit 4:4:4 RGB +HS\VS\CLK,输出为YPBPR。
在输入信号为720P的时候,输出YPBPR正常。
但是我需要的输入信号为800X480,转换为YPBPR就异常,用示波器测试YPBPR有信号,但是后端接的显示器无法显示。
请问THS8200在显示720P和800X480的信号,有哪些不同的寄存器呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
//THS8200 480p Generic Mode
WR_REG,THS8200,0x01,0x03,0x11 // chip_ctl
WR_REG,THS8200,0x01,0x1C,0x60 // dman_cntl
WR_REG,THS8200,0x01,0x1D,0xFF // dtg_y_sync1
WR_REG,THS8200,0x01,0x1E,0x50 // dtg_y_sync2
WR_REG,THS8200,0x01,0x1F,0xFF // dtg_y_sync3
WR_REG,THS8200,0x01,0x20,0xFF // dtg_cbcr_sync1
WR_REG,THS8200,0x01,0x21,0xFF // dtg_cbcr_sync2
WR_REG,THS8200,0x01,0x22,0xFF // dtg_cbcr_sync3
WR_REG,THS8200,0x01,0x23,0x11 // dtg_y_sync_upper
WR_REG,THS8200,0x01,0x24,0x15 // dtg_cbcr_sync_upper
WR_REG,THS8200,0x01,0x25,0x3D // dtg_spec_a
WR_REG,THS8200,0x01,0x26,0x10 // dtg_spec_b
WR_REG,THS8200,0x01,0x27,0x20 // dtg_spec_c
WR_REG,THS8200,0x01,0x28,0x7A // dtg_spec_d
WR_REG,THS8200,0x01,0x29,0x00 // dtg_spec_d1
WR_REG,THS8200,0x01,0x2A,0xC0 // dtg_spec_e
WR_REG,THS8200,0x01,0x2B,0x01 // dtg_spec_h_msb
WR_REG,THS8200,0x01,0x2C,0x90 // dtg_spec_h_lsb
WR_REG,THS8200,0x01,0x2D,0x03 // dtg_spec_i_msb
WR_REG,THS8200,0x01,0x2E,0x1B // dtg_spec_i_lsb
WR_REG,THS8200,0x01,0x2F,0x10 // dtg_spec_k_lsb
WR_REG,THS8200,0x01,0x30,0x00 // dtg_spec_k_msb
WR_REG,THS8200,0x01,0x31,0x00 // dtg_spec_k1
WR_REG,THS8200,0x01,0x32,0xAD // dtg_speg_g_lsb
WR_REG,THS8200,0x01,0x33,0x01 // dtg_speg_g_msb
WR_REG,THS8200,0x01,0x34,0x03 // dtg_total_pixel_msb
WR_REG,THS8200,0x01,0x35,0x5A // dtg_total_pixel_lsb
WR_REG,THS8200,0x01,0x36,0x80 // dtg_linecnt_msb
WR_REG,THS8200,0x01,0x37,0x08 // dtg_linecnt_lsb
WR_REG,THS8200,0x01,0x38,0x85 // dtg_mode
WR_REG,THS8200,0x01,0x39,0x27 // dtg_frame_field_msb
WR_REG,THS8200,0x01,0x3A,0x0D // dtg_frame_size_lsb
WR_REG,THS8200,0x01,0x3B,0xFF // dtg_field_size_lsb
// CSM set to map reduced YCbCr range to DAC Full-scale
WR_REG,THS8200,0x01,0x41,0x40 // csm_clip_gy_low
WR_REG,THS8200,0x01,0x42,0x40 // csm_clip_bcb_low
WR_REG,THS8200,0x01,0x43,0x40 // csm_clip_rcr_low
WR_REG,THS8200,0x01,0x44,0xAC // csm_clip_gy_high
WR_REG,THS8200,0x01,0x45,0xAC // csm_clip_bcb_high
WR_REG,THS8200,0x01,0x46,0xAC // csm_clip_rcr_high
WR_REG,THS8200,0x01,0x47,0x40 // csm_shift_gy
WR_REG,THS8200,0x01,0x48,0x40 // csm_shift_bcb
WR_REG,THS8200,0x01,0x49,0x40 // csm_shift_rcr
WR_REG,THS8200,0x01,0x4A,0xDC // csm_mult_gy_msb
WR_REG,THS8200,0x01,0x4B,0x44 // csm_mult_bcb_rcr_msb
WR_REG,THS8200,0x01,0x4C,0xAB // csm_mult_gy_lsb
WR_REG,THS8200,0x01,0x4D,0x91 // csm_mult_bcb_lsb
WR_REG,THS8200,0x01,0x4E,0x91 // csm_mult_rcr_lsb
WR_REG,THS8200,0x01,0x4F,0xF5 // csm_mode
WR_REG,THS8200,0x01,0x70,0x40 // dtg_hlength_lsb
WR_REG,THS8200,0x01,0x71,0x03 // dtg_hdly_msb
WR_REG,THS8200,0x01,0x72,0x31 // dtg_hdly_lsb
WR_REG,THS8200,0x01,0x73,0x07 // dtg_vlength_lsb
WR_REG,THS8200,0x01,0x74,0x00 // dtg_vdly_msb
WR_REG,THS8200,0x01,0x75,0x07 // dtg_vdly_lsb
WR_REG,THS8200,0x01,0x76,0x00 // dtg_vlength2_lsb
WR_REG,THS8200,0x01,0x77,0xC7 // dtg_vdly2_msb
WR_REG,THS8200,0x01,0x78,0xFF // dtg_vdly2_lsb
WR_REG,THS8200,0x01,0x79,0x00 // dtg_hs_in_dly_msb
WR_REG,THS8200,0x01,0x7A,0x0F // dtg_hs_in_dly_lsb use to adjust horizontal alignment
WR_REG,THS8200,0x01,0x7B,0x00 // dtg_vs_in_dly_msb
WR_REG,THS8200,0x01,0x7C,0x00 // dtg_vs_in_dly_lsb use to adjust vetical alignment
WR_REG,THS8200,0x01,0x82,0x03 // pol_cntl exterrnal FID
END_DATASET