This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DAC5675a的输入时钟电平的问题

Other Parts Discussed in Thread: DAC5675A

在手册里写DAC5675a的clk输入可以使用单端,即clk输入cmos电平信号,clkc端通过电容接地,内部通过电阻网络接到2/3 AVdd

但是在digital specifications里面写的【clk-clkc】的范围是min 0.4,max 0.8,这样cmos的单端输入时clk-clkc很容易超过这个范围。

而且还有一点是在手册的figure 18里,写:node CLKC internally Biased to AVdd/2 可是怎么看Figure 14里面都是2/3 AVdd啊,是手册标错了还是我理解错了?

  • 1. 你说的没错,如果是5V CMOS或者2.5V CMOS都会超出400mV ~800mV的范围,数据手册里的CMOS应该指的1.5VCMOS。里面也提到还兼容LVPECL单端输入,LVPECL的幅值正好为800mV,所以是没问题的。

  • “node CLKC internally Biased to AVdd/2 ”这个应该是打印错误,按照Figure16 的clock内部框图可以看出CLKC的电压应该是2/3 AVDD.

  • 你好,首先谢谢您的耐心解答

    但还有有些疑问,看图他是直流耦合进入clk端的,并不是交流耦合,且内部有2,2v的偏置,如果按手册说明Vpp<0.8v,clkc端确定是2,.2v, 则clk端应该是高电平2.6V,低电平1.8V,这个显然也不是1,5vcmos的电平标准,更类似3.3Vlvttl。

     手册写的很模糊,据同事说用lvcmos确实能驱动,但是本着谨慎期间还是期待权威人士能给一些说明。

  • 确实很模糊,我刚忘记CLKC内部有2.2V偏置,这样的话,不是1.5V LVCMOS电平了,如果在400~800mV的幅值范围内的话,那么Voh(max)=2.6V,Vol(min)=1.8V,Voh(min)=2.4V,Vol(max)=2V. 也就是说Voh在2.4V~2.6V范围内,Vol在1.8V~2V范围内,这样看来不是标准的TTL或者CMOS电平。但这样的分析应该是没问题的。

  • 主要是我们想知道,虽然他的极限输入时-0.3到AVdd+0.3,但如果长时间使用lvcmos电平驱动这个芯片,会不会引起clk管脚的失效。

    谢谢

  • 使用任何一款TI的器件,电气特性都不要参考你说的极限输入,需要参考数据手册中的“Recommend Electrical Characteristics"保证芯片性能。

    所以对DAC5675A也一样。CLK ,CLKC的共模电压为2V+20%,幅值为400~800mV。 即Voh=2.6V,Vol=1.8V和Voh=2.4V和Vol=2V范围内。

  • 麻烦问一下,我现在使用5675A,时钟引脚CLK接到3.3V的CMOS电平上,CLKn通过电容连接到地上,DA输出的时钟为150MHZ,由FPGA提供,FPGA在时钟下降沿打入数据,上升沿开始转换。有时候DA输出有毛刺,和两个时钟引脚的差值400mv-800mv不满足有关系吗?