您好,我在电路设计时遇到的问题是:
前面一个模块采用高压10V电源供电,输出方式为单端输出,输出信号范围为5±4V,而后端输入为3.3V电源供电,采用全差分的输入方式,输入范围为1.65V±0.75V。两个模块之间需要一个接口电路,用于实现单端到差分,及电压范围变换的功能,TI有推荐的方案没?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在电路设计时遇到的问题是:
前面一个模块采用高压10V电源供电,输出方式为单端输出,输出信号范围为5±4V,而后端输入为3.3V电源供电,采用全差分的输入方式,输入范围为1.65V±0.75V。两个模块之间需要一个接口电路,用于实现单端到差分,及电压范围变换的功能,TI有推荐的方案没?谢谢!
比例缩小时,在电路中是否可以实现共模电压从5V转变为1.65V,同时前面模块的输出范围从5±4V 完整缩放到1.65±0.75V呢?
我的理解是:把5V电压缩减到1.65V,同样1V/9V缩减对应的比例,到0.33V/2.97V?这与1.65±0.75V的范围无法完整对应,请问我的理解是否有错误?
比例缩小时,在电路中是否可以实现共模电压从5V转变为1.65V,同时前面模块的输出范围从5±4V 完整缩放到1.65±0.75V呢?
我的理解是:把5V电压缩减到1.65V,同样1V/9V缩减对应的比例,到0.33V/2.97V?这与1.65±0.75V的范围无法完整对应,请问我的理解是否有错误?
全差分运放输出共模电压可以设置,你设置为1.65就好了。比例缩小4/0.75倍就得到了你的+/-0.75V